cancel
Showing results for 
Search instead for 
Did you mean: 

How to set this RCC_RDCR reigster for bootrom?

Daniel-0723
Associate
  • MCU: STM32N6
  • Register: RCC reset duration control register (RCC_RDCR)
    • Bits 27:24 EADLY[3:0]: External access delay
      The bit field is security-protected by the 1 bit. Set and reset by software.
      Time to wait before the BOOTROM performs any external device access
      0000: No extra delay added by the BOOTROM
      0001: 100 μs
      0010: 200 μs
      0011: 500 μs
      0100: 1 ms
      0101: 2 ms
      0110: 5 ms (default after reset)
      0111: 10 ms
      1000: 20 ms
      1001: 50 ms
      1010: 100 ms
      1011: 200 ms
      1100: 500 ms
      1101: 1 s
      1110: 2 s
      1111: 5 s
 

 

 
 
 

 

 

 

1 REPLY 1
Amel NASRI
ST Employee

Hi @Daniel-0723 ,

I assume that it remains as default value (5ms) if you don't change it.

Based on the article STM32N6 boot ROM explained provided by @B.Montanari and UM3234 How to proceed with boot ROM on STM32N6 MCUs, I don't see a particular setup for this register.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.