2018-03-14 6:41 AM
Hello,
I am new for stm32 (nucleo-f429zi) and truestudio. I try new stm32cube_fw_f4_v1.21.0. when I try example of new firmware. I can't set includes path and directories correctly. After 2 days work, I can include all .h and .c, but complier can't identify path to find stm32f4xx_nucleo_144.h although I add the path in setting ' path and directories'. I find some instruction to use example in truestudio, but after I follow all steps, I still can't make any example work. Does anybody can present how to set default path and directories for nucleo-f429zi in latest truestudio?
2018-03-14 8:00 AM
These things are a lot easier to trouble shoot if you a) show the exact error messages you are seeing, and b) show the 'Include Paths' you are supplying the tool chain with.
2018-03-14 10:05 AM
Clive One wrote:
show the exact error messages you are seeing,
Probably also show the actual line(s) of source code that are giving those error messages
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.