2016-03-25 9:33 PM
Hi All,
I would like to send uint32_t hex via USART, but no idea how to do it.for example:uint32_t buffer[2];buffer[0] = 0x12345678;buffer[1] = 0x87654321;USART_puts(buffer[0]) <-- ???? the USART_puts length is uint8_t not 32-bitvoid USART_puts(uint8_t * data){ uint8_t u_i=0; while(data[u_i]!='\0') { USART_SendData(USART6, data[u_i++]); while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET); }}Thank you.2016-03-25 10:48 PM
Hello,
in order to keep the USART_puts function as is (send 8bit characters), I propose you to create an intermediate function which will split the buffer of 32bit elements to a buffer of 8bit elements.A simple function to do this would be:void splitbuffer(uint32_t* buf32bit,uint8_t* buf8bit){ int i; for (i=0;i<sizeof(buf32bit)/4;i++) { buf8bit[4*i+0]=(buf32bit[i]>>24)&0xFF; buf8bit[4*i+1]=(buf32bit[i]>>16)&0xFF; buf8bit[4*i+2]=(buf32bit[i]>>8)&0xFF; buf8bit[4*i+3]=(buf32bit[i])&0xFF; }}and you would call it by:splitbuffer(buffer32bit,buffer8bit);(remember to declare a buffer8bit[] array with four times the number of elements of buffer32bit.How the function works is quite simple:- The for loop runs for every element of the 32bit buffer after determining its size (sizeof returns the size of the 32bit buffer in bytes and each element is 4 bytes long).- For every element a shifting is performed starting from the Most Significant Byte (>>24) with a bitwise AND to isolate the specific byte.- The final 8bit buffer is little endian, meaning that the most significant byte is at the first position and the least significant byte is at the last position.2016-03-26 3:16 AM
void USART_buffer(uint8_t * data, size_t size)
{
while(size--)
{
while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET);// Check it is empty FIRST
USART_SendData(USART6, *data++);
}
}
USART_buffer((void *)buffer, sizeof(buffer));
USART_puts(buffer[0]); // INCORRECT, buffer[0] is NOT a pointer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.