2022-11-18 1:16 AM
Hi,
I am working on stm32f051c8t6tr microcontroller, from this I want to read some sensor data with UART1 and same data I want to transmit to another UART. Can you please suggest some example code related to my task. I am new to this controller.
I have tried one code also but its not working, I will share the code in below
HAL_UART_Receive(&huart1,(uint8_t *)buffer,10,10);
HAL_UART_Transmit(&huart2,(uint8_t *)buffer,10,10);
The above two line of code only I tried, buts its not giving any output; Please help me on this.
2022-11-21 10:38 AM
First test your sensor with bluetooth HC-05 or similar from a pc.
If this passes, implement a sw fifo tx and rx between both uart to be clean. Use byte uart interrupt. Gas sensor are usually slow response time, high bitrate probably not needed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.