2011-12-12 2:40 PM
Hello. I want to read a sequence of bytes from my accelerometer. I can't get it work.
When I read byte by byte all is ok, but when I try to read sequence I can't get a true values.void ADXL_ReadSeq(uint8_t StartAddr,signed char *data)
{ // StartAddr |= (1<<7); // while(I2C_GetFlagStatus(I2CG, I2C_FLAG_BUSY)); // While the bus is busy I2C_GenerateSTART(I2CG, ENABLE); // Send START condition while(!I2C_CheckEvent(I2CG, I2C_EVENT_MASTER_MODE_SELECT)); // Test on EV5 and clear it I2C_Send7bitAddress(I2CG, DEV_ADDR<< 1, I2C_Direction_Transmitter); // Send address for write (SAD+W) while(!I2C_CheckEvent(I2CG, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); // Test on EV6 and clear it I2C_SendData(I2CG,ADXL_R| ADXL_MB|StartAddr ); //Multibyte reading while(!I2C_CheckEvent(I2CG, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // Test on EV8 and clear it I2C_GenerateSTART(I2CG, ENABLE); // Send STRAT condition a second time while(!I2C_CheckEvent(I2CG, I2C_EVENT_MASTER_MODE_SELECT)); // Test on EV5 and clear it I2C_Send7bitAddress(I2CG, DEV_ADDR<< 1, I2C_Direction_Receiver); // Send address for read while(!I2C_CheckEvent(I2CG,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Test on EV6 and clear it int i=0; for (i;i<6;i++) { I2C_AcknowledgeConfig(I2CG, ENABLE); data[i]=I2C_ReceiveData(I2CG); delay(3000); } I2C_AcknowledgeConfig(I2CG, DISABLE); I2C_GenerateSTOP(I2CG, ENABLE); // Send STOP Condition}What I'm doing wrong?I convert this function from other function which uses SPIhttp://code.google.com/p/flyless/source/browse/trunk/FLYLess/src/hal/adxl345.c
#i2c #sequence #adxl345 #stm322011-12-13 9:33 AM
When I read byte by byte all is ok, but when I try to read sequence I can't get a true values.
assuming you are using stm32f1xx read the errata Erik
2011-12-13 9:33 AM
When I read byte by byte all is ok, but when I try to read sequence I can't get a true values.
assuming you are using stm32f1xx read the errata Erik
2011-12-13 9:49 AM
Yes, I have stm32f103vet6. But I don't know where to search. Please help me.I'm getting data normally, but not data that I need.
2011-12-13 10:31 AM
as said before READ THE ERRATA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.