cancel
Showing results for 
Search instead for 
Did you mean: 

How to program STM32 -Using I2C to control SAA1064 ;4-digits LED driver Hello,

fifi
Associate

Hello,

I would like to program the STM32 to control the circuit SAA1064 by I2C, using the STM32cubeIDE and HAL functions (HAL_I2C_Mem_Write,HAL_I2C_Master_Transmit, HAL_I2C_IsDeviceReady). then with the function "HAL_I2C_IsDeviceReady" shows that : the I2C communication is OK,  but I can't send data to the SAA1064 to display the digits on 7segments.

thank you for helping 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @fifi, to the community!

Please show us the programme you have written so far. Are there also pull-ups on the lines?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.