2020-05-20 7:09 AM
I'm using the arm_rfft_fast_f32 function, I write a scatter file and place some library files in the CCM SRAM like below, and the speed is faster.
RW_IRAM2 0x10000000 0x00002800 { ; CCM SRAM 10kB
.ANY (ccmram)
arm_rfft_fast_f32.o (+RO)
arm_cfft_f32.o (+RO)
arm_cfft_radix8_f32.o (+RO)
arm_rfft_fast_init_f32.o (+RO)
}
but the twiddleCoef tables in arm_common_tables.o are too large to fit into the CCM SRAM, how to place the table "twiddleCoef_256" into the CCM SRAM specifically? Other tables are useless in my app.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.