2019-01-12 3:57 AM
I am going to use STM32F030k6t6. IC is not having VBAT pin. Please suggest how to make RTC active when power is off
2019-01-12 7:47 AM
The 'F030 is a cut-down version of the 'F031/'F051, with some features deliberately left off.
In other words, you have to chose an STM32 model which has the VBAT pin.
JW
2019-01-13 8:38 PM
Dear Waclawek.jan sir,
Thanks for your reply .
I want to know is there any solution to use stm32f030k6t6 as clock. As i want to make cost effective application.
2019-01-14 12:08 AM
You can have an external switchover (maybe just a diode or two) from primary power source to battery, and write the software so that if primary source goes away the mcu goes into some of the low-power mode.
However, the battery consumption will be higher than it would be using a mcu with VBAT pin.
jW
2019-01-14 1:37 AM
Please share the details or link about how to deal with low power modes for respective microcontroller. it will be very helpful for me
2019-01-15 2:18 PM
Isn't STM32L010K4 or similar chips more appropriate, if energy consumption and low power modes are important? The price is approximately the same. Are there some other special requirements?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.