2019-11-06 6:27 AM
hi, I use the official example to change, the example need two board(one master and one slave), I am tring to make spi master and slave communication in one board, My board stm32f411ve. I use PortB13~15(spi2) and3~5(spi3), when I set both of spi2 and spi3 to be master, and MOSI connect to itselfs MISO, its work, and the value is right. When I set one of them to slave, MOSI(PB15)-MOSI(PB5) MISO(PB14)-MISO(PB4) SCK(PB3)-SCK(PB13)and it will time out error. this is my code.
#define MASTER_BOARD
/* Private variables ---------------------------------------------------------*/
/* SPI handler declaration */
SPI_HandleTypeDef SpiHandle;
SPI_HandleTypeDef SpiHandle2;
/* Buffer used for transmission */
uint8_t aTxBuffer[] = "****SPI - Two Boards communication based on Polling **** SPI Message ******** SPI Message ******** SPI Message ****";
/* Buffer used for reception */
uint8_t aRxBuffer[BUFFERSIZE];
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void Error_Handler(void);
static void Timeout_Error_Handler(void);
static uint16_t Buffercmp(uint8_t* pBuffer1, uint8_t* pBuffer2, uint16_t BufferLength);
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program
* @param None
* @retval None
*/
int main(void)
{
/* STM32F4xx HAL library initialization:
- Configure the Flash prefetch, instruction and Data caches
- Configure the Systick to generate an interrupt each 1 msec
- Set NVIC Group Priority to 4
- Global MSP (MCU Support Package) initialization
*/
HAL_Init();
/* Configure LED3, LED4, LED5 and LED6 */
BSP_LED_Init(LED3);
BSP_LED_Init(LED4);
BSP_LED_Init(LED5);
BSP_LED_Init(LED6);
/* Configure the system clock to 100 MHz */
SystemClock_Config();
/*##-1- Configure the SPI peripheral #######################################*/
/* Set the SPI parameters */
SpiHandle.Instance = SPIx;
SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;
SpiHandle.Init.CLKPolarity = SPI_POLARITY_HIGH;
SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle.Init.CRCPolynomial = 7;
SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle.Init.NSS = SPI_NSS_SOFT;
SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE;
#ifdef MASTER_BOARD
SpiHandle.Init.Mode = SPI_MODE_MASTER;
//SpiHandle.Init.Mode = SPI_MODE_SLAVE;
#else
SpiHandle.Init.Mode = SPI_MODE_SLAVE;
#endif /* MASTER_BOARD */
if(HAL_SPI_Init(&SpiHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
SpiHandle2.Instance = SPI3;
SpiHandle2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle2.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle2.Init.CLKPhase = SPI_PHASE_1EDGE;
SpiHandle2.Init.CLKPolarity = SPI_POLARITY_HIGH;
SpiHandle2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle2.Init.CRCPolynomial = 7;
SpiHandle2.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle2.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle2.Init.NSS = SPI_NSS_SOFT;
SpiHandle2.Init.TIMode = SPI_TIMODE_DISABLE;
#ifdef MASTER_BOARD
SpiHandle2.Init.Mode = SPI_MODE_SLAVE;
//SpiHandle2.Init.Mode = SPI_MODE_MASTER;
#else
SpiHandle2.Init.Mode = SPI_MODE_MASTER;
#endif /* MASTER_BOARD */
if(HAL_SPI_Init(&SpiHandle2) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
#ifdef MASTER_BOARD
/* Configure Tamper push button */
BSP_PB_Init(BUTTON_KEY, BUTTON_MODE_GPIO);
/* Wait for Tamper Button press before starting the Communication */
while (BSP_PB_GetState(BUTTON_KEY) != 1)
{
BSP_LED_Toggle(LED3);
HAL_Delay(40);
}
BSP_LED_Off(LED3);
#endif /* MASTER_BOARD */
/*##-2- Start the Full Duplex Communication process ########################*/
/* While the SPI in TransmitReceive process, user can transmit data through
"aTxBuffer" buffer & receive data through "aRxBuffer" */
/* Timeout is set to 5S */
switch(HAL_SPI_TransmitReceive(&SpiHandle2, (uint8_t*)aTxBuffer, (uint8_t *)aRxBuffer, BUFFERSIZE, 5000))
{
case HAL_OK:
/* Communication is completed_____________________________________________*/
/* Compare the sent and received buffers */
if(Buffercmp((uint8_t*)aTxBuffer, (uint8_t*)aRxBuffer, BUFFERSIZE))
{
/* Transfer error in transmission process */
Error_Handler();
}
/* Turn LED4 on: Transfer in transmission process is correct */
// BSP_LED_On(LED4);
/* Turn LED6 on: Transfer in reception process is correct */
BSP_LED_On(LED6);
break;
case HAL_TIMEOUT:
/* A Timeout occurred______________________________________________________*/
/* Call Timeout Handler */
Timeout_Error_Handler();
break;
/* An Error occurred_______________________________________________________*/
case HAL_ERROR:
/* Call Timeout Handler */
Error_Handler();
break;
default:
break;
}
switch(HAL_SPI_TransmitReceive(&SpiHandle, (uint8_t*)aTxBuffer, (uint8_t *)aRxBuffer, BUFFERSIZE, 5000))
{
case HAL_OK:
/* Communication is completed_____________________________________________*/
/* Compare the sent and received buffers */
if(Buffercmp((uint8_t*)aTxBuffer, (uint8_t*)aRxBuffer, BUFFERSIZE))
{
/* Transfer error in transmission process */
Error_Handler();
}
/* Turn LED4 on: Transfer in transmission process is correct */
BSP_LED_On(LED4);
/* Turn LED6 on: Transfer in reception process is correct */
// BSP_LED_On(LED6);
break;
case HAL_TIMEOUT:
/* A Timeout occurred______________________________________________________*/
/* Call Timeout Handler */
Timeout_Error_Handler();
break;
/* An Error occurred_______________________________________________________*/
case HAL_ERROR:
/* Call Timeout Handler */
Error_Handler();
break;
default:
break;
}
/* Infinite loop */
while (1)
{
}
}
THANKS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.