2016-10-03 5:46 AM
Hi.
I would like to implement MPU for stack overflow detection. I suppose that I should know in advance where the boundaries of stack and heap are.
Is it possible to read these boundaries from C code? Or is it possible to define exact region which will be reserved for stack and heap?
I know I can set stack and heap size in startup file, but there is no definition for top of the stack (or bottom of the heap).
Thank you
#i-accept-paypal2016-10-03 5:55 AM
Define and export symbols for the things you want to see. Doesn't the top of stack get exported as __initial_sp, the base as Stack_Mem ? And the heap as __heap_base (Heap_Mem), __heap_limit ?
2016-10-03 8:37 AM
Hmm, I don't really understand what you want to say... Do you have any piece of code to show?
2016-10-03 9:10 AM
I'd have to write. Please review the linker/symbol stuff provided to you last week. [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/CRC%20calculation%20over%20code%20in%20Flash&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%3D20160930%252013%253a29%253a31%26p_ID%3D70358%26View%3D%257bF47A9ED8%252dE726%252d42BE%252dACED%252d732F13B66581%257d%26FolderCTID%3D0x012001%26PageFirstRow%3D41¤tviews=48]Here
Review the concepts around assemblers/linkers/loaders in the context of your tool-chainhttp://www.keil.com/support/man/docs/armasm/armasm_dom1361290009343.htm
http://www.keil.com/support/man/docs/armasm/armasm_dom1361290016692.htm
et al The linker's job is to fix up symbols in the name-space. The C and ASM files share the same name-space, and you can reference them, and have the linker do it's job and associate them automatically. The public symbols are also typically provided in the .MAP and .ELF/AXF object files.2016-10-03 9:22 AM
From startup_stm32fxxx.s, and *EXPORT* the symbols you want to reference elsewhere
...
Stack_Size EQU 0x00000400
AREA STACK, NOINIT, READWRITE, ALIGN=3
Stack_Mem SPACE Stack_Size
__initial_sp
; <
h
> Heap Configuration
; <
o
> Heap Size (in Bytes) <
0x0-0xFFFFFFFF:8
>
; </
h
>
Heap_Size EQU 0x00000200
AREA HEAP, NOINIT, READWRITE, ALIGN=3
__heap_base
Heap_Mem SPACE Heap_Size
__heap_limit
PRESERVE8
THUMB
; Vector Table Mapped to Address 0 at Reset
AREA RESET, DATA, READONLY
EXPORT __Vectors
EXPORT __Vectors_End
EXPORT __Vectors_Size
__Vectors DCD __initial_sp ; Top of Stack
DCD Reset_Handler ; Reset Handler
...
2016-10-03 11:11 AM
Hi Clive,
I know that I was asking similar things previous week. Things which I was asking there works perfectly now. Now, I tried to read stack size and top address in a similar manner, but without success.I will read the links that you suggested.I appreciate your help every time.2016-10-04 11:05 AM
Now, I am able to read exported __initial_sp value in c file. There were two things which were causing problems:
1. I didn't have enabled MicroLIB and there is ''IF DEF'' in startup file which exports__initial_sp only if MicroLIB is enabled. IF :DEF:__MICROLIB
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
ELSE
IMPORT __use_two_region_memory
EXPORT __user_initial_stackheap
__user_initial_stackheap
LDR R0, = Heap_Mem
LDR R1, =(Stack_Mem + Stack_Size)
LDR R2, = (Heap_Mem + Heap_Size)
LDR R3, = Stack_Mem
BX LR
ALIGN
ENDIF
END
Thus, I deleted ''
IF :DEF:__MICROLIB'' and
everything between ''ELSE'' and ''ENDIF''. 2. I tried to read__initial_sp as:extern
uint32_t __initial_sp;
uint32_t Value;
Value = __initial_sp;
Instead of:
extern
uint32_t __initial_sp;
uint32_t Value;
Value = (uint32_t)&__initial_sp;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.