2018-03-08 2:32 AM
spwf01sc wifi module so that it is permanently store in the internal flash. For example the default files available as below when issued 'at+s.fsl ' command.
I 461 /input_demo.shtml
I 384 /output_demo.html
I 614 /index.html
I 157 /peers.shtml
I 193 /config.shtml
I 180 /message.shtml
I 174 /status.shtml
I 5496 /remote.html
I 3447 /firstset.html
I 212 /404.html
Thanks & Regards
Jitendra NVS
2018-03-12 7:14 AM
In SPWF01S wifi module, could perform File system update using AT+S.HTTPDFSUPDATE over the air with the help of Apache web server successfully (from Lab6 of Wi-Fi Training - Hands On manual).
But the same is giving problem using UART
(from Lab6 of
Wi-Fi Training - Hands On manual)
after the below commands:• AT+S. HTTPDFSWRITE=357957
• In Tera Term: File – Send File...Not prompting to issue a reset command in order to complete the file system update, but hanging in the mid. Please help me in solving this issue.
Thanks & Regards
Jitendra NVS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.