2023-05-21 4:15 PM
MacOS has evolved out from under the STM32CubeProgrammer for Mac installation process again. This issue was dealt with for an earlier version of macOS. Looking at this earlier posting, I was able to install the Programmer app from the command line, but with two issues:
FYI, here's the version of JRE I have installed:
% java -version
openjdk version "20.0.1" 2023-04-18
OpenJDK Runtime Environment Temurin-20.0.1+9 (build 20.0.1+9)
OpenJDK 64-Bit Server VM Temurin-20.0.1+9 (build 20.0.1+9, mixed mode, sharing)
% I presume the current installation procedure will involve some variant of the earlier CLI process. Recommendations?
TIA
Mike
2023-05-21 7:08 PM
As a partial answer to my question, a useful hint can be found in the ReadMe file for the Cube MX app:
In case of error, try one of the following fixes: - $sudo xattr -cr ~/SetupSTM32CubeMX-6.8.1.appFor the current case, using the command line, go to the folder containing the Setup app and execute:
sudo xattr -cr SetupSTM32CubeProgrammer-2.13.0.appThen run the Setup... app. It will run OK, but complain that it can't install in the /Applications folder. The recommended alternative, my Users home folder, works, but is a rather strange place to put a macOS app. The app won't show up in Launchpad; you'll have to put a link to it somewhere handy that you can double-click on.
Recommendations:
Thanks,
Mike
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.