2018-01-24 5:00 PM
Hi I'm new with stm32, I bought an stm32f0discovery but I can't work with it I wanna get help or some tutorial please.
2018-01-29 4:38 AM
Nidhal Abidi wrote:
I find it a bit difficult to start with
So did you look at the 'basic getting-started tips' I linked as the very first reply?
2018-01-29 4:43 AM
Nidhal Abidi wrote:
Arduino avr is not as arm ones.
AVR is not fundamentally different from ARM; it's just a difference in scale - not in fundamental principles.
See:
https://community.st.com/0D50X00009XkWm7SAF
2018-01-29 5:36 AM
Note that STM32 is now supported directly in the Arduino IDE:
Previously, there were a number of 'Arduino-like' things - including
https://www.leaflabs.com/maple/
, , the above-mentioned '', et al ...2018-01-29 1:35 PM
Hey could I use the integrated st-link v2 in the stm32f0discovery to flash or to program something else or other chip. It exists 6 pins (SWD) ???
2018-01-29 2:40 PM
http://www.st.com/resource/en/user_manual/dm00050135.pdf
4.2chapter Using
ST-LINK
/V2 to program/d ebug an external ST M32 application2018-01-29 2:54 PM
Thanks I did read it but how. Is it possible to flash arduino via the ' ISP header 6-pins' ???
2018-01-29 3:00 PM
On the top of information provided by Andrewlet me share with you a presentation, which guides how to get started step by step with STM32 and Arduino IDE. Please find a file attached.
Regards
Szymon ________________ Attachments : STM32_Arduino.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy4s&d=%2Fa%2F0X0000000b3q%2FxG_rFACqZ0QHduA.ww2JpseEwzmlXTV9.lmllDjm8bQ&asPdf=false2018-01-29 5:37 PM
It will only program other STM32s.
2018-01-29 11:24 PM
Excellent guide! Now, two things must be addressed in the future:
1 - markings on the Nucleo boards for all 5V tolerant pins (Microchip has a migration guide from 5V to 3.3V, do you have something similar?) - you can't imagine how useful is this for the person that come from the 8bit/5Vcc microcontrollers that still have a plethora of 5Vcc peripherals on his cabinet and in fact, continue to develop for those micros (every time he hits his head on an STM32 specific problem);
2 - the Arduino/Wiring language implemented over the LL driver - having it implemented on the HAL is just ridiculous! HAL itself is already a 'Wiring language'. It can make a real difference in the Arduino world, so don't be so stingy...
2018-01-30 2:28 AM
Vasile Guta_Ciucur wrote:
It can make a real difference in the Arduino world
Well, it's all open source - so, if you think it should be done, get on and do it!
don't be so stingy...
Indeed!
:)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.