2025-05-10 8:43 PM
Given that my QSPI driver and external loader for the W25Q128JVSIQ are already working, is there a hidden CubeProgrammer/DFU-descriptor trick that lets the stock USB bootloader read/write my external QSPI flash at 0x90000000, or must I build a custom USB-DFU bootloader that:
Initializes QSPI and advertises the 0x90000000 region
Handles read/write/erase transfers
so I can flash firmware onto the external flash over USB? If I do go the custom route, can I still use CubeProgrammer for the update, or do I need to write my own host application?
Solved! Go to Solution.
2025-05-30 3:25 AM
Hi @AhmedSayed
STM32 built-in bootloader does not support the update of an external flash (using USB DFU or any other interface), it only supports the update of internal memory (Flash, RAM, OTP, RO, EEPROM, OB..). It should be feasible using custom bootloader to handle external flash programming.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-30 3:25 AM
Hi @AhmedSayed
STM32 built-in bootloader does not support the update of an external flash (using USB DFU or any other interface), it only supports the update of internal memory (Flash, RAM, OTP, RO, EEPROM, OB..). It should be feasible using custom bootloader to handle external flash programming.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.