2018-06-15 3:15 AM
Hi, I have read the AN4852 application note explaining how to program an external QSPI flash using the built-in UART bootloader. However it does not tell how to execute afterwards the code saved in the external flash on the microcontroller. Does the microcontroller somehow have to read the code and copy it into internal flash or how could it be done?
#external-flash #code #stm32f407 #execute Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-06-15 3:46 AM
The 'classic' 'F4xx don't have facility to run code from QSPI, so you'd need either to copy it into internal FLASH or internal RAM (except the CCM RAM) and run it from there.
Newer families, such as the 'L4 and 'F7, and the upper-end and lower-end 'F4, have a QSPI controller which can be part of the memory map and code can be run directly from there.
JW
2018-06-15 6:18 AM
Ok, thank you. And is there any kind of 'easy' way of copying the code into internal flash?
2018-06-15 8:17 AM
The 'easier' way would be to memcpy() it to RAM and jump to it there.
The QSPI support in some of the F4 and F7 parts maps the external memory into the address space of the processor (0x90000000), and from there you can jump to it like any other code, and execute-in-place (XIP)
External memory on the F4 parts is not remotely fast or cached.
On the F42x/F43x parts you can use SDRAM, as I recall thats about 6x slower to access than internal SRAM.
It is not that 'hard' to erase/write internal FLASH, one could certainly construct a 'memcpy' type function to achieve it.
2018-06-15 8:49 AM
The QSPI support in some of the F4 and F9 parts
Any insider, forward information on the 'F9s?
;)
(yes I know it's a typo but couldn't resist, sorry)
Jan
2018-06-15 10:05 AM
Yeah, my brain was already at the 0x900... part of the sentence and working its way to my fingers
They are working on a multi-core H7 which is why the single core seems to be getting no attention at the moment
2018-06-18 12:19 AM
So there is not a memcpy() function to copy code into flash but just using the custom functions from HAL to do so. I've read that first the flash must be unlocked before erasing or writing to it. Why is this? Just curious.
Another issue, my binary file would be a .elf instead of a .bin, does it matter? Because I've seen that .bin files are purely binary but .elf files have more things such sections, symbols, relocateable table for address offsets and so.
2018-06-18 3:10 AM
So there is not a memcpy() function to copy code into flash but just using the custom functions from HAL to do so.
You can write your own...
flash must be unlocked before erasing or writing to it. Why is this?
This is some sort of a safeguard, so that it's less likely that some runaway piece of code would make things worse by overwriting unintentionally the FLASH.
Another issue, my binary file would be a .elf instead of a .bin, does it matter?
Extract the relevant binary from .elf using objcopy, e.g. (depending on your particular toolchain)
'[path to toolchain]\bin\arm-none-eabi-objcopy' -O binary main.elf main.bin
JW
2018-06-25 2:31 AM
I've been studying how the bootloader of this uC works and it needs something which sends the commands and data through UART, from which I understand that the uC itself cannot autoboot and copy the code by itself. I was thinking about putting a PIC and make this send the data from a FRAM to the STM, but by doing this the system will depend on the flash of the PIC instead of the FRAM. Is there any approach on autobooting the STM?
2018-06-25 7:46 AM
What does 'auto-booting' mean?
The STM32 can reset itself, it can jump into ROM, you can have a small loader in FLASH that always runs and load data from an external source. Trying to understand the necessity of a PIC in all this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.