2021-09-23 11:03 AM
I'm wondering if the following is correct for using the ART flash accelerator on the STM32F7 line:
We don't program the flash from application, so is it best to use ITCM with ART or AXIM and enable caching?
2021-09-23 11:09 AM
@Sylvie Boube-Politano
2021-09-23 1:16 PM
I think I've got it now:
For future people: you leave the Flash Latency set as described in the reference manual.
The second half of the dm above helped a lot, plus finding and studying the matching code at:
2021-09-23 1:51 PM
>>For future people: you leave the Flash Latency set as described in the reference manual.
Yes, because the flash array has a fixed (slow, say 35ns) speed which needs to be accommodated in CPU clock cycles, that the synchronous design also uses for the ART and FLASH interfacing logic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.