2019-03-08 6:14 AM
Hi,
I don't find how to configure this DMA mode with CubeMx. This mode seems not mentioned in AN4031 (application note for DMA controler).
I want to implement it on a nucleo F429ZI board. I'm working with CubeMx + TrueStudio.
Best
2019-03-14 3:51 AM
Now I have to connect this signal to DMA2 to trigger the frame, and configure DMA. It'll be harder than the timer. And in fact, i realise that cubeMx is not necessary the easier way to configure register.
I'll be back to you if I got problem to configure the DMA. But I first try alone reading different AN.
Best
2019-03-22 2:34 AM
I don't find how to connect the DMA1 output to a GPIO, I supposed that is by choosing the right Alternate Function of the GPIO, but I don't find the DMA AF. In the project mentioned, they useDMA1 and PORTB MSB [15-8] with only [11-8] realy used. I don't understand how they do that.
Consequently, I'm not enable to determine all the GPIO usable as output for the DMA1 used as memory-to-gpio mode.
Can you help me?
Best
2019-03-22 4:09 AM
In STM32F4xx, DMA1 can't access GPIO, only DMA2 can.
> In the project mentioned
I don't know what project are you talking about, but it might've been a different STM32 family.
This has nothing to do with AF. DMA just moves data from or to GPIO, so GPIO is set as input or output respectively.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.