2021-01-20 9:38 PM
Hi, i am controlling my stepper motor by giving commands through modbus in stm32f103. I am able to drive motor in one direction . But i am not able to drive my motor in another direction by sending command through modbus.
can anyone please help me with it.
i have another confusion whether i need to give negative values from my modbus to drive motor in another direction or not please anyone help me with it.
Thank you
2021-01-20 10:24 PM
You have two options. The first is to encode direction in the 16-bit register used to specify the speed or number of steps. A positive register setting (0x0000-off, 1-0x7fff move positive direction) specifies clockwise stepping. A negative (0xffff-0x8000, 1 to 0x7fff in negative direction) specifies counterclockwise.
If you need the full 16-bit value for step count then use a one-bit register to select clockwise/counterclockwise direction. The disadvantage here is it now takes two commands to start the motor.
Jack Peacock
2021-01-20 10:31 PM
To add to Jack's correct answer - the modbus protocol does not "know" of positive/negative values.
It only specifies single bits and register (16-bit) values.
The signedness is in the interpretation of the sender/receiver (master and slave in modbus terms).
2021-01-21 12:45 AM
if(motion_type_absolute > 0 && motion_type_absolute < 65535 ) // positive direction
{
set direction pin as set;
}
else if(motion_type_absolute >32767 && motion_type_absolute < 65536) //negative direction
{
set direction pin as reset;
}
is this correct logic can i add to my code to drive stepper motor in both direction.
Thank you
2021-01-21 12:46 AM
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.