2011-02-02 1:12 PM
How to calculate tan angles..
2011-05-17 5:23 AM
add ''math.h'' lib and use tan(x) function.
2011-05-17 5:23 AM
Use the tan(x) from your C compiler.
2011-05-17 5:23 AM
''add 'math.h' lib''
Note that math.h is
not
a library - it is just a header file! In addition to #include-ing math.h, you will also have to add the appropriate floating-point lirary/libraries to your project. For details, see the documentation for your particular toolset. Note that some free/restricted toolset versions may not allow use of floating point2011-05-17 5:23 AM
@neil: I am using Ride7 and working on STM32F103ZE. Do you know how to add that floating library file in it?? is it available for this controller?. Thanks a lot for help.
2011-05-17 5:23 AM
Note that floating-point has a very significantly greater overhead (both code size and execution time) than integer maths - therefore you should think very carefully indeed whether you really need floating point in your application.
This is one reason why many (most?) embedded toolchains do not include floating-point by default. In most cases, it is easy enough to scale you values so that you can do everything in integer maths; eg, instead of processing 3.3V as a floating-point number, think of it as 3300mV - an integer! You can choose any scaling factor that is convenient to your particular application. Functions such as tan() can be implemented as lookup tables, or integer implementations - so-called ''fixed point'' - are available. eg, CORDIC algorithms:http://en.wikipedia.org/wiki/CORDIC
So, try it first using floating-point; but be aware that this may give you code-size and/or performance issues - so be prepared to explore the alternatives...2011-05-17 5:23 AM
If you want to learn more about methods and approximations, have a look at the book ''Math toolkit for real-time programming'' by Jack W. Crenshaw.
2011-05-17 5:23 AM
Integer vs. floating point makes a BIG difference in execution time. My DTMF decode went from 10 milliseconds to 0.6 milliseconds.
This was for a 100 sample Goertzel algorithm performing sums and power calculation using integer arithmetic returning a signed 64-bit integer. I used 16 different frequencies -- the basic 8(*) and their second harmonics. C code converted that to 32-bit fp. Column/row selection used fp to pick a winner that had to be 3x the sum of the other three items. Sum of all 8 harmonics had to be a factor of 3 or 4 less than the winning row value. (*) that included the almost never present ABCD column to the right of 369#.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.