2019-11-20 8:51 AM
I am using the NUCLEO-144 (STM32H743ZI) board. It contains the following memory regions:
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
All I would like to do is assign the data section to RAM_D2 and the bss section to RAM_D2. The issue is when I set the data section to RAM_D2 in the linker script, the application I build hard faults (InvState Error) on the following instruction in the startup script:
/* Call static constructors */
bl __libc_init_array
The following is how I am assigning memory to data and bss sections:
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM_D2 AT> FLASH
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM_D1
Is there an issue with alignment?
Solved! Go to Solution.
2019-11-20 1:31 PM
2019-11-20 1:29 PM
Some of the H7 SRAM needs its clock enabled before use, otherwise it will fault.
2019-11-20 1:31 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.