2012-05-24 1:11 AM
Please, could you help me? with STM32F4xx.
But I think it's general problem with GNU linker.
I'm working on SW for colour graphical display application.
It works fine.
But I need to store some data to Flash after the program start.
I want allocate for this data all 16K Sector 1 in Flash area.
I have tried different ways but unsuccessfully.
My variable is
const unsigned
short
int
FlashArray[8192].
I have tried this:
const unsigned short
int
FlashArray[8192] __attribute__ ((at((uint32_t)0x08004000)));This doesn't work in GNU.
I have tried also this:
const
unsigned
short
int
FlashArray[8192]
__attribute__
((section(
''.flash_data_array''
)));
+
change in stm32_flash.ld:
/* Specify the memory areas */
MEMORY
{
FLASH0 (rx) : ORIGIN = 0x08000000, LENGTH = 16K
FLASH1 (rx) : ORIGIN = 0x08004000, LENGTH = 16K
FLASH2 (rx) : ORIGIN = 0x08008000, LENGTH = 992K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
MEMORY_B1 (rx) : ORIGIN = 0x60000000, LENGTH = 0K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH0
/* My new eeprom area in FLASH */
.flash_data_array :
{
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} >FLASH1
?
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH2
...
But this doesn't work too.
I don't know what's wrong.
I have tried to found out it on internet, but without success.
Here I found out this problem has more people.
Can you help me how to allocate variable array to Sector1 in Flash
and how to prohibit this sector to other flash data?
#linker2014-06-18 1:16 AM
Sorry I forgot to include it, now is in attachment.
Once again thanks for Your help.2014-06-18 10:53 AM
With my own startup/link script examples I didn't see the problem. Based on RIDE GNU/GCC implementation
I was able to duplicate the issues by creating an equivalent startup.s and customizing it for the STM32F4 I used Chuck's framework here which seemed compatible with your script as a starting point.http://robotics.mcmanis.com/src/arm-blink/cm4_startup_code.html
In order to get the vectors to emit properly I changed the following: .section .isr_vector,''a'',%progbits ________________ Attachments : startup.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1A4&d=%2Fa%2F0X0000000bj9%2FT2Deo4eXg7nASQTRKqPSWSfvMTlIMjL6MILEek0t3U8&asPdf=false2014-06-19 1:45 AM
Sorry I forgot to include it, now is in attachment.
Do you have '.isr_vector' section defined in your startup?I can only see '.isr' int he attached elf.You can try to rename it to '.isr' in the linker script or '.isr_vector' section in startup file.
2014-06-19 5:33 AM
I don't have his startup.s, and it's different to the RIDE one, but when I made an equivalent it had
.section .isr_vector which wasn't sufficient to keep the vectors. This was using Yagarto 4.7.22014-06-24 2:09 AM
I include start-up file in attachment. It has declaration of section '.isr_vector'. Please look at it. Basicly it's code taken from samples which comes with ARM GCC compiler. I have just edited the contents of the isr table to adapted it to STM32 family.
I don't think that is a start-up problem because like I mention before when i add *(.text.SD*) *(.text.*Handler) Program runs ok and isr table is allocated in right place. Any ideas what can by wrong? ________________ Attachments : startup_STM32F40XX.S : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I19z&d=%2Fa%2F0X0000000bjA%2FBSI9Du93f3U8ToQNSls1mMv0GrlI4n.fVxmSQhcUyks&asPdf=false2014-06-25 1:50 AM
As Clive mentioned you need to change this line in your startup:
.section .isr_vector
to
.section .isr_vector,''a'',%progbits
2014-06-25 8:12 AM
2015-02-13 4:49 PM
I'm trying to get this sort of thing to work. SofarI have:
in a .c file__attribute__((__section__(
''.user_data''
)))
const
int32_t userConfig[32];
and inan .lds file:
ENTRY(Reset_Handler)
MEMORY
{
FLASH (RX) : ORIGIN = 0x08000000, LENGTH = 1022k
DATA (RX) : ORIGIN = 0x080FF7FF, LENGTH = 2k
SRAM (RWX) : ORIGIN = 0x20000000, LENGTH = 112K
SRAM2 (RWX) : ORIGIN = 0x2001c000, LENGTH = 16K
CCM (RWX) : ORIGIN = 0x10000000, LENGTH = 64K
BACKUP_SRAM (RWX) : ORIGIN = 0x40024000, LENGTH = 4K
}
_estack = 0x2001c000;
SECTIONS
{
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector))
. = ALIGN(4);
} > FLASH
.user_data :
{
. = ALIGN(4);
*(.user_data)
. = ALIGN(4);
} > DATA
.text :
{
. = ALIGN(4);
_stext = .;
*(.text)
*(.text*)
*(.rodata)
*(.rodata*)
*(.glue_7)
*(.glue_7t)
KEEP(*(.init))
KEEP(*(.fini))
. = ALIGN(4);
_etext = .;
} > FLASH
.ARM.extab :
{
. = ALIGN(4);
*(.ARM.extab)
*(.gnu.linkonce.armextab.*)
. = ALIGN(4);
} > FLASH
.exidx :
{
. = ALIGN(4);
PROVIDE(__exidx_start = .);
*(.ARM.exidx*)
. = ALIGN(4);
PROVIDE(__exidx_end = .);
} > FLASH
.ARM.attributes :
{
*(.ARM.attributes)
} > FLASH
.preinit_array :
{
PROVIDE(__preinit_array_start = .);
KEEP(*(.preinit_array*))
PROVIDE(__preinit_array_end = .);
} > FLASH
.init_array :
{
PROVIDE(__init_array_start = .);
KEEP(*(SORT(.init_array.*)))
KEEP(*(.init_array*))
PROVIDE(__init_array_end = .);
} > FLASH
.fini_array :
{
PROVIDE(__fini_array_start = .);
KEEP(*(.fini_array*))
KEEP(*(SORT(.fini_array.*)))
PROVIDE(__fini_array_end = .);
} > FLASH
. = ALIGN(4);
_sidata = .;
.data : AT(_sidata)
{
. = ALIGN(4);
_sdata = .;
PROVIDE(__data_start__ = _sdata);
*(.data)
*(.data*)
. = ALIGN(4);
_edata = .;
PROVIDE(__data_end__ = _edata);
} > SRAM
.bss :
{
. = ALIGN(4);
_sbss = .;
PROVIDE(__bss_start__ = _sbss);
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .;
PROVIDE(__bss_end__ = _ebss);
} > SRAM
PROVIDE(end = .);
}
I can't seem to be able to read back the correct value after writing to this location with
HAL_FLASH_Program(TYPEPROGRAM_WORD, &userConfig[0], somedata);
2015-02-13 7:02 PM
Surely 0x080FF800 ? Although the flash block up there is 128KB in size, so you'd want to watch what the erase does, and what address you're actually using.
Can't help you with the HAL stuff. You could trying dumping the memory area in question, and checking what's there before/after you do things. ie dumpdata(0x800, (void *)0x080FF800); Check also the error/status returns for the flash functions, or query the flash peripheral directly.2015-02-14 3:00 AM
sorry, 80FF800 is correct. Turns out that I hadn't been erasing the sector before writing (nothing mentioned in the hal library about this) This code works now:
__attribute__((__section__(
''.userdata''
)))
const
int32_t userConfig[32];
...
...
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR);
FLASH_Erase_Sector(FLASH_SECTOR_11, VOLTAGE_RANGE_3);
HAL_FLASH_Program(TYPEPROGRAM_WORD, &userConfig[MAGICNUMBER_LOC], MAGICNUMBER);
HAL_FLASH_Lock();
My ld file is now set as so:
MEMORY
{
FLASH (RX) : ORIGIN = 0x08000000, LENGTH = 1M-128K
DATA (RWX) : ORIGIN = 0x080E0000, LENGTH = 128k
SRAM (RWX) : ORIGIN = 0x20000000, LENGTH = 112K
SRAM2 (RWX) : ORIGIN = 0x2001c000, LENGTH = 16K
CCM (RWX) : ORIGIN = 0x10000000, LENGTH = 64K
BACKUP_SRAM (RWX) : ORIGIN = 0x40024000, LENGTH = 4K
}
Now I want to move the DATA to sector 0 as I don't need the 128k space and would benefit from faster erase speeds. If I try
MEMORY
{
FLASH (RX) : ORIGIN = 0x08004000, LENGTH = 1M-16K
DATA (RWX) : ORIGIN = 0x08000000, LENGTH = 16k
SRAM (RWX) : ORIGIN = 0x20000000, LENGTH = 112K
SRAM2 (RWX) : ORIGIN = 0x2001c000, LENGTH = 16K
CCM (RWX) : ORIGIN = 0x10000000, LENGTH = 64K
BACKUP_SRAM (RWX) : ORIGIN = 0x40024000, LENGTH = 4K
}
The application wont even start anymore. I get errors in the upload processing saying ''could not write to 0x8000000 at offset 0x4000'' and various other things. Why can I use sector 11 and not sector 0?
Also what do the suffuses (RX), (RWX) mean?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.