2017-08-17 9:47 PM
RCC->APB1ENR |= (1<<28);
PWR->CR |= (PWR_CR_VOS);
RCC->CR |= (1<<0);
RCC->CR |= (RCC_CR_HSICAL_4); //
Internal high-speed clock calibration
RCC->CFGR |= RCC_CFGR_SW_HSI; //
HSI oscillator selected as system clock
RCC->CFGR |= RCC_CFGR_PPRE2_DIV2; //
APB high-speed prescaler (APB2)
RCC->CFGR |= RCC_CFGR_PPRE1_DIV4; //
APB Low speed prescaler (APB1)
RCC->CFGR |= RCC_CFGR_HPRE_DIV1; //
AHB prescaler
RCC->CR &= ~(1<<24); //
PLL OFF
RCC->PLLCFGR &= ~(1<<22); //
HSI clock selected as PLL
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLM;
RCC->PLLCFGR |= RCC_PLLCFGR_PLLM_4; //
Division factor for the main PLL (PLL) input clock (16)
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLN;
RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_4; //
Main PLL (PLL) multiplication factor for VCO (336)
RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_6;
RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_8;
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLP;
RCC->PLLCFGR |= RCC_PLLCFGR_PLLP_1; // Main PLL (PLL) division factor for main system clock(2)
RCC->CR |= (1<<24); // enable PLL
while(!(RCC->CR & RCC_CR_PLLRDY)); // waiting for PLL lock
RCC->CFGR |= RCC_CFGR_SW_PLL; // PLL_P selected as system clock
Above code shows configuration to achieve maximum system clock (168MHz) , but during running time on keil uvision5 compiler shows 'cannot access memory' . Please suggest a method to solve this issue .......
#stm32f446-system-clock2017-08-18 3:56 AM
Are you sure Keil's complaint is related to these lines? Are you trying to access external memory with the debugger? (I don't use Keil so these are blind shots)
JW
2017-08-18 7:01 AM
Yikes! That's hideously inefficient code, thought the point of this level of programming was to be minimal/optimal.
You'll need wait states for the FLASH
You'll want to avoid errata/hazards of enabling clocks and immediately touching the same peripheral.
Bunch of assumptions about initial conditions.
2017-08-19 2:05 AM
This code work for system clock upto 142MHz by changing the value of PLL_N . On increasing further, error 'Cannot access memory' arises.
I am using STM32F446 Nucleo 144 Board.
2017-08-19 7:27 AM
{
uint32_t pll_n = 360, pll_p = 2, pll_m = 16, pll_q = 7, pll_r = 7;RCC->APB1ENR |= RCC_APB1ENR_PWREN;
RCC->CFGR |= RCC_CFGR_HPRE_DIV1 | /* HCLK = SYSCLK / 1*/
RCC_CFGR_PPRE2_DIV2 | /* PCLK2 = HCLK / 2*/ RCC_CFGR_PPRE1_DIV4; /* PCLK1 = HCLK / 4*//* Select regulator voltage output Scale 1 mode, System frequency up to 168..180 MHz */
PWR->CR |= PWR_CR_VOS;/* Configure the main PLL */
RCC->PLLCFGR = pll_m | (pll_n << 6) | (((pll_p >> 1) - 1) << 16) | (RCC_PLLCFGR_PLLSRC_HSI) | (pll_q << 24) | (pll_r << 28);RCC->CR |= RCC_CR_PLLON; /* Enable the main PLL */
while((RCC->CR & RCC_CR_PLLRDY) == 0); /* Wait till the main PLL is ready */
/* Enable the Over-drive to extend the clock frequency to 180 Mhz */
PWR->CR |= PWR_CR_ODEN; while((PWR->CSR & PWR_CSR_ODRDY) == 0); PWR->CR |= PWR_CR_ODSWEN; while((PWR->CSR & PWR_CSR_ODSWRDY) == 0);/* Configure Flash prefetch, Instruction cache, Data cache and wait state */
FLASH->ACR = FLASH_ACR_ICEN | FLASH_ACR_DCEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_6WS; // 5WS Might work/* Select the main PLL as system clock source */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW)); RCC->CFGR |= RCC_CFGR_SW_PLL;/* Wait till the main PLL is used as system clock source */
while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS ) != RCC_CFGR_SWS_PLL);}2017-08-23 11:47 PM
Thank You Clive .Maximum clock frequency (180MHz) achieved when enabling over drive and FLASH .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.