2020-01-20 7:15 AM
I hope the title tells it but F746 was out of stock in a couple of European stockists and H750 was in stock and also cheaper. Both in LQFP100. I wonder am I lucky or do I have to make a new board? If buggy forum permits, that is.
Solved! Go to Solution.
2020-01-20 1:33 PM
I copied settings my self from CPU to CPU. It looks like they are pin compatible.
2020-01-20 7:52 AM
The F746, F756 and F750 should all be the same die/bondout. The latter having CRYPT/HASH enabled, and less memory tested.
2020-01-20 9:51 AM
I'm pretty sure the H7s are not pin compatable with the F7 series. They are also quite abit more complicated and the H750 only has one sector of flash.
2020-01-20 9:54 AM
Sorry read F7, ST and their F750 H750 naming to confuse everyone.
I'd walk down the Data Sheet columns for the 100-pin devices in both chips. Have boards where we're run 144-pin H7 and F7 interchangeably.
2020-01-20 10:15 AM
I chose the 100 pin version. Too bad. I have to check those datasheets, sometimes it is just faster to get an answer from forum.
2020-01-20 10:52 AM
Power supply, special pins and ports are similar. I wonder, can ports be programmed similarly too, I mean can I have timers, uarts, ADC and so on at same pins.
,
2020-01-20 1:33 PM
I copied settings my self from CPU to CPU. It looks like they are pin compatible.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.