2022-05-04 11:20 AM
Only want to pair with OOB data in SC mode (nothing else)
Have already called aci_gap_set_oob_data(0, 0, 0, 0, 0, 0) to gen OOB data
Have got said data from aci_gap_get_oob_data
Paring packets show the OOB data bit is not set.
aci_gap_set_authentication_requirement(
)
To see the packet on windows the device currently lies that it has a yes/no display but that should not affect the OOB data bit being set to present.
Solved! Go to Solution.
2022-05-04 11:46 AM
I missed this but it appears that the bit is used to let the a device know that its OOB data has been passed and is being used in the pairing.
I will test and post if that is correct.
2022-05-04 11:46 AM
I missed this but it appears that the bit is used to let the a device know that its OOB data has been passed and is being used in the pairing.
I will test and post if that is correct.
2022-05-12 9:41 AM
For anyone who might find this: I will not be testing. A little more research found that IOS does not appear to support OOB (for none apple devices) at this point.Note that Android does but only via NFC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.