2017-12-26 2:39 AM
Hi,
Iam using an stm32F746 nucleo board and run the web server example with Netconn RTOS.
Working fine, IP is given and samples html files are loaded.
However the ethernet cable disconnection is not being detected (shouldnt the red led be ON?) and the worst thing is that when the cable is back the software is stuck and needs restart.
Any ideas how to overcome this deadlock?
2017-12-26 3:19 AM
How do you detect an ethernet cable disconnection?
By polling the PHY regularly.
JW
2017-12-26 8:40 AM
Thanks, no doubt that I should poll regurarly
However seems that after initializations for RTOS, TCP/IP etc the main never executes....It is stated on the code also.
Why is that?
int main(void)
{....
.....
osThreadDef(Start, StartThread, osPriorityNormal, 0, configMINIMAL_STACK_SIZE * 5);
osThreadCreate (osThread(Start), NULL); /* Start scheduler */ osKernelStart(); /* We should never get here as control is now taken by the scheduler */ <------ for( ;; ){ User_notification(&gnetif); <------this never executes...... };}2017-12-26 7:46 PM
I am new to all this stuff too..
I am having some aberrations on Ethernet as you are; locking up the Ethernet functions until hard reset.
I started with the cube.
my code is like yours;
We never exit the RTOS task sharing program called osStartKernel();
//Create user task
task = osCreateTask('run HTTP Tasks', httpTask, NULL, 8*1024, OS_TASK_PRIORITY_NORMAL);//Failed to create the task?
if (task == OS_INVALID_HANDLE) { // osCreateTask httpTask has failed with OS_INVALID_HANDLE // Error(); } //Start the execution of tasks osStartKernel(); // Error: 1st osStartKernel shouldn't ever exit, but it did. We should never get here// This function should never get here
for (;;) ;2017-12-28 2:09 PM
I have a similar issue,
as per your suggestion, I have tried to read the phy, but getting the wrong answer.
PHY BSR : 0x782d
PHY BCR : 0x3100 PHY SR : 0x0002 MAC Address : 02:AB:CD:EF:07:67 Rx mode : Interrupts Negotiation : Disabled Speed : undefined Duplex : Half LAN84710A status : READY Link status : Upis this correct ?
uint32_t phyBSR;
HAL_ETH_ReadPHYRegister(heth, PHY_BSR, &phyBSR); sprintf(etherString, ' PHY BSR : 0x%04x\r\n', phyBSR);how can I read the BSR directly, without the HAL ReadPHYRegister function ?
2017-12-29 12:08 AM
Is the cable disconnected?
If yes i assume the answer is not correct
I will check it this afternoon on my board and let you know
Στις 28 Δεκ 2017 23:10, ο χ�?ήστης 'marsh.nick' <
st-microelectronics@jiveon.com> έγ�?αψε:
STMicroelectronics Community
<https://community.st.com/?et=watches.email.thread>
Re: How do you detect an ethernet cable disconnection?
reply from marsh.nick
<
MCUs Forum* - View the full discussion
<https://community.st.com/0D70X000006SvwMSAS
2017-12-29 12:20 PM
Hi Nick,
At my case I always get a LinkStatus =0 (down) even if the cable is connected.
The code that is working in my case is as follows, check better the phyreg , works like a ''charm'' in my Nucleo board.
Don't ask me if I can get UP the Ethernet interface, I am just playing with indication Leds at the moment.
Regards
/Kostas
static void MonitorThread(void const * argument)
{ for(;;){ EthHandlefGlobal=get_ethernet_handle(); heth=&EthHandlefGlobal; //pointer to Global Variable /* We wait for linked status */ HAL_Delay(PHY_RESET_DELAY); HAL_ETH_ReadPHYRegister(heth, PHY_BSR, &phyreg); if((phyreg & PHY_LINKED_STATUS) != PHY_LINKED_STATUS){ //link is down, red light BSP_LED_On(LED3); BSP_LED_Off(LED1);} else { //link is up, green light BSP_LED_Off(LED3); BSP_LED_On(LED1); } }}2017-12-30 1:34 PM
I tried to read the PHY, but I am getting the wrong values.
how would you read it?
this doesn't work..
uint32_t phyBSR;
HAL_ETH_ReadPHYRegister(heth, PHY_BSR, &phyBSR); sprintf(etherString, ' PHY BSR : 0x%04x\r\n', phyBSR);reporting : PHY BSR : 0x782d <- this does not seem correct
:(
2017-12-31 12:50 AM
hi,
In my board I am getting these values:
connected ethernet cable: phyreg=0x780d
disconnected ethernet cable: phyreg=0x7809
I have the NUCLEO-F746ZG mb 1137 rev b
the PHY should be LAN8742A_PHY_ADDRESS (i don't know where exactly in the board is..)
set a breakpoint inside stm32f7xx_hal_eth.c at line
317 } while (((phyreg & PHY_LINKED_STATUS) != PHY_LINKED_STATUS));
and check the phyreg with and without the cable.
2017-12-31 8:50 PM
I have found a problem in my code and fixed it, I am using the LAN8710A
you should check this in your code;
stm32f7xx_hal_conf.h
#define PHY_SR ((uint16_t)31) /*!< PHY status register Offset */ //this is now corrected
#define PHY_SR ((uint16_t)0x31) /*!< PHY status register Offset */ //this is wrong
finally, I can confirm MII mode and 100MHz operation,
but only one led stays on, I dont see any flickers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.