2019-04-05 7:41 AM
Hello everyone
how config timer 1 to trigger timer 3 every fall edge on PWM channel 1 and channel 2
2019-04-12 7:41 AM
Hello @Pedram ,
It's not possible to trigger the timer 3 from timer 1 through channel 1 and channel 2 in the same time.
The source of trigger output of timer1 should be one of these:
You can refer to the "Timer synchronization" section in the reference manual relevant to your device.
Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.