2020-06-07 6:42 AM
I want to use STM32 as ECU(VCU) for my formula student Electric Vehicle. I am using Orion BMS and DTI motor controller.
2020-06-07 11:44 AM
This is a very broad question.
In general, you should plan out what the things you need in the ECU and evaluate if a STM32 chip can do these. A good way to start would be to list all the interfaces to external devices that you need to support.
You've listed two of these. I see the DTI needs an RS232 input. The STM32 can't do this directly, but you can use a chip to convert between the single ended UART signal and the RS232 signal.
If you have no experience with the STM32, a good starting point would be to pick up a Nucleo board, flash some LEDs on it, and then move on to implementing the higher-level functionality that you need.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.