2018-03-25 11:18 PM
hi
i have tried a lot to config pwm in stm32f103re with IAR but i could not do that activity.
i put the code here to get help from you guys . i am really confused.
please tell me my problem in code , and where i am wrong.
thanks a lot.&sharpinclude 'stm32f10x.h'
&sharpinclude 'stm32f10x_gpio.h' // for Enable LCD&sharpinclude 'stm32f10x_rcc.h' //for Enable LCD&sharpinclude 'stm32f10x_tim.h'&sharpinclude 'LCDLib.h'&sharpinclude 'delay.h'void tim_init(void);void GPIO_init(void);int main(){ lcd_init(); lcdPutString ('Believe Your Dreams.'); tim_init(); GPIO_init(); while(1){ } }void tim_init(){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; TIM_TimeBaseStructure.TIM_Prescaler = 8; TIM_TimeBaseStructure.TIM_Period = 500; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); TIM_Cmd(TIM3, ENABLE); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 400; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC4Init(TIM3, &TIM_OCInitStructure); TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);//GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_TIM4);
}void GPIO_init(void){ RCC_APB2PeriphClockCmd ( RCC_APB2Periph_GPIOC, ENABLE ); GPIO_InitTypeDef gpioAa; gpioAa.GPIO_Mode = GPIO_Mode_AF_PP ; gpioAa.GPIO_Pin = GPIO_Pin_9; gpioAa.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init( GPIOC, &gpioAa ); }#pwm2018-03-26 5:54 AM
Would probably do a more complete job of initializing the pin.
Also with PC9 at TIM3_CH4 you'd need to enable the AFIO clock and Remap TIM3 pin usage. Review pin remapping details in Reference Manual RM0008
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.