2018-10-24 11:24 PM
Please suggest code and setup to test all low power modes supported by the STM32L4 controller series and Nucleo-4R5ZI development kit
2018-10-24 11:47 PM
If you had a well known resistor, say 2.00 ohms(1% or 0.1%) and put that in series from the power supply to the board, then measure the voltage across it...
ie V=IR,
I = V/R
use a multi meter...
2018-10-25 12:14 AM
Hi Nick,
Thank you for the response, i am unable to test Low power sleep mode code on the Nucleo-4R5ZI development kit. I am using kit and switch as mentioned.
I just want to know is anything else required to test low power mode code?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.