2019-07-29 7:39 AM
I am working with the STM32F446 microcontroller and I need to detect when a 50 Hz (plus-minus 2 Hz) square wave signal is turned on and off, respectively. The signal is connected to a pin that has TIMx_CHy alternate functionality. Is there a way to accomplish this without having to handle roughly 50 interrupts/second?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.