2022-06-15 1:48 AM
I tried to get the minium delay between output state but I am limited by the GPIO toggling speed, I even tried PWM generation and there is an option on GPIO settings -> Maximum output speed but I can't change it by clicking on it.
Does anybody has an idea on how to set up the maximum speed for GPIO Output?
2022-06-15 2:03 AM
This is essentially the same question you asked here. It's probably clearer to finish discussing the topic there and stay in one thread.
Regards
/Peter
2022-06-15 2:04 AM
Okay no problem
2022-06-15 2:06 AM
It's just that my question here is more precise
2022-06-15 2:39 AM
@Peter BENSCH
It's probably clearer to finish discussing the topic there and stay in one thread.
All very well, Peter. But someone has marked that question as answered so those who feel able to help might not look at it to see there's a supplementary question
2022-06-15 2:44 AM
> there is an option on GPIO settings -> Maximum output speed but I can't change it by clicking on it
This to me sounds like question on CubeMX and its quirks and limitations.
JW
2022-06-15 2:50 AM
Thank you for having replied to my question in the other topic
2022-06-15 2:51 AM
You're right
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.