2021-02-19 12:08 AM
I have about 250 mikroAmpere current consumption in shutdown mode.
used board: NUCLEO-G474RE, nothing except ammeter connected to the board.
code to shutdown:
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_DisableWakeUpPin (PWR_WAKEUP_PIN2_HIGH);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnableWakeUpPin (PWR_WAKEUP_PIN2_HIGH);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWREx_EnterSHUTDOWNMode();
the same code on a nucleo f411 schows 2 uA as expected. only the G474 board show this high current.
our application board with g474 show the same high current.
if I heat the board up, the current is not increasing!
what can be the problem?
Is something special with g474?
thanks
Martin
2021-02-19 3:38 AM
I read again the datasheet and 250 mikroampere (IDD(wakeup from shutdown)) is quite normal, because the wakeup logic runs with 16 MHz.
That is very ugly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.