cancel
Showing results for 
Search instead for 
Did you mean: 

Hi,Is it possible to load hex file of STM32F746ZGT6 in to STM32F756ZGT6? need to program directly using utility

adham.1
Associate

A hex file generated from STM32F746ZGT6 is it compatible with STM32F756ZGT6?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
adham.1
Associate

thank you so much...!

You're welcome. Please close this thread by clicking "Select as best" in the answer.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Perhaps mark the actual answer to the question as the best, rather than your response.

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.