2021-11-04 3:47 AM
I tryed two methodes, one just jumping to that address 0x1fff0000 via function pointer and second writing some magic numbers at 0x2001fffc and placing some asm code in the startup *.s file to jump branch to the system bootloader. I had to change controller typ recently. Before that i had the stm32f105 worked perfectly.
Here parts of my code
*.s file
/* Call the clock system intitialization function.*/
bl SystemInit
/* check for a magic number in RAM, if present */
/* branch to bootloader */
LDR R0, =0x2001fff8
LDR R1, =0x12345678
LDR R2, [R0, #0]
STR R0, [R0, #0]
CMP R2, R1
BEQ Bootloader
/* Call static constructors */
bl __libc_init_array
/* Call the application's entry point.*/
bl main
bx lr
.size Reset_Handler, .-Reset_Handler
/* Start systemmemory bootloader */
Bootloader:
LDR R0, =0x1fff0000
LDR SP, [R0, #0]
LDR R0, [R0, #4]
BX R0
it does not stay in bootloader and in windows device manager could not see the device as an dfu bootloader device.
rest of code
void JumptoSysMem()
{
volatile uint32_t addr = boot_addr;
USB_OTG_GlobalTypeDef *USBx = hpcd_USB_OTG_FS.Instance;
//Enumeration_USB();
USB_DevDisconnect(USBx);
HAL_Delay(1000);
HAL_RCC_DeInit();
HAL_DeInit();
SysTick->CTRL = 0;
SysTick->VAL = 0;
SysTick->LOAD = 0;
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
__set_MSP(*(uint32_t *)addr);
#if 0
SysMemBootJump = (void (*) (void)) (*((uint32_t *)(addr + 4)));
SysMemBootJump();
#else
//place magic at flash address 0x2001fffc
volatile uint32_t * magic_number_addr = (uint32_t *)0x2001fff8;
*magic_number_addr = magic_number;
__NVIC_SystemReset();
#endif
while(1);
}
what am i doing wrong please give me some detailed information.
Thanks in advance
2021-11-04 6:15 AM
Here's how to jump to bootloader on the F4:
https://stm32f4-discovery.net/2017/04/tutorial-jump-system-memory-software-stm32/
Looks to be the same as what you're doing. If that's not working, you'll need to debug further. Ensure hardware watchdog isn't enabled. If it doesn't stay in the bootloader, figure out where it's going. If it's resetting, look at RCC->CSR bits to determine why. If you have other signals active, it may be jumping to those bootloaders rather than USB DFU.
2021-11-04 7:44 AM
Hi,
thanks for answering. i have disabled my watchdog for now and still it does not stay in dfu bootloader it always start appliation. I also capture the RCC->CSR = 0x14000000 and all the time i like to jump i get this result. I do not have any other signals that could trigger a dfu bootloader.
2021-11-04 8:22 AM
You should use the method as I originally posted it.
The System Memory needs to be remapped in the assembler function, it doesn't survive the reset.
One of the purposes of the reset is to clear up whatever non-sense state the application left the processor/system in.
;*****************************************************************************
ALIGN
Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0]
LDR R0,[R0, #4]
BX R0
ENDP
;*****************************************************************************#PoorlyPlagarised
2021-11-05 1:29 AM
Hi,
i placed your code into mine with no better result. It still jumps to somewhere and just starts again the application.
In my opinion i do a clean up before jumping but not with my assembler code but with the c code. Both are not working. The only way to get there is to set the BOOT1 jumper, but that is not sufficient for me. Any advice.
Thanks for reply
2021-11-05 6:50 AM
Hi,
one thing to add. When usb cable is not connected to the PC the bootloader runs. But as soon you plug in the usb cable it starts the application and does not initialize as a dfu device.
Please could you give me some hint because i am stucked right now.
Thanks
2021-11-08 1:52 AM
Hi,
i was able to stay in bootloader for now by just adding the disable_irq() that had been missing. But now got error code 43 in device manager. it could not get any device descriptor. But when placing a jumper to BOOT0 pin it is recognising as an stm32 Bootloader?
Any ideas?
Thanks
2021-11-08 6:07 AM
Everything you've described can be explained by the vector table not pointing to the correct location. USB DFU requires interrupts be enabled.
2021-11-08 6:18 AM
Hi,
i had also tried to switch the vector table but i not sure if had done that right.
SCB->VTOR = VECT_TAB_BASE_ADDRESS | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM. */
VECT_TAB_BASE_ADDRESS ---> address?
VECT_TAB_OFFSET ---> offset?
When placing the system memory to address 0x00000000 via macro and placed the vector table to that also
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
SCB->VTOR = 0x00000000;
I tried this did not work either.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.