2020-06-19 10:50 AM
I have got error like this can you please let me know how to resolve this error.
make: *** No rule to make target '../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_spi.c', needed by 'Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_spi.o'. Stop.
2020-06-19 7:22 PM
Clean the build, then rebuild.
Check if that file exists.
Re-generate the code in CubeMX.
2020-06-20 12:59 AM
Thanks for the reply.
I have clean the build and rebuild , i got error like this.
Description Resource Path Location Type
'SPI_BAUDRATEPRESCALER_64' undeclared (first use in this function) main.c /vent_cont/Core/Src line 378 C/C++ Problem
'SPI_CRC_LENGTH_DATASIZE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 383 C/C++ Problem
'SPI_CRC_LENGTH_DATASIZE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 412 C/C++ Problem
'SPI_CRCCALCULATION_DISABLE' undeclared (first use in this function); did you mean 'SPI_TIMODE_DISABLE'? main.c /vent_cont/Core/Src line 381 C/C++ Problem
'SPI_CRCCALCULATION_DISABLE' undeclared (first use in this function); did you mean 'SPI_TIMODE_DISABLE'? main.c /vent_cont/Core/Src line 410 C/C++ Problem
'SPI_DATASIZE_8BIT' undeclared (first use in this function); did you mean 'I2C_MEMADD_SIZE_8BIT'? main.c /vent_cont/Core/Src line 374 C/C++ Problem
'SPI_DATASIZE_8BIT' undeclared (first use in this function); did you mean 'I2C_MEMADD_SIZE_8BIT'? main.c /vent_cont/Core/Src line 404 C/C++ Problem
'SPI_DIRECTION_2LINES' undeclared (first use in this function); did you mean 'I2C_DIRECTION_RECEIVE'? main.c /vent_cont/Core/Src line 373 C/C++ Problem
'SPI_DIRECTION_2LINES' undeclared (first use in this function); did you mean 'I2C_DIRECTION_RECEIVE'? main.c /vent_cont/Core/Src line 403 C/C++ Problem
'SPI_FIRSTBIT_MSB' undeclared (first use in this function); did you mean 'SPI_SR_BSY_Msk'? main.c /vent_cont/Core/Src line 379 C/C++ Problem
'SPI_FIRSTBIT_MSB' undeclared (first use in this function); did you mean 'SPI_SR_BSY_Msk'? main.c /vent_cont/Core/Src line 408 C/C++ Problem
'SPI_MODE_MASTER' undeclared (first use in this function); did you mean 'HAL_I2C_MODE_MASTER'? main.c /vent_cont/Core/Src line 372 C/C++ Problem
'SPI_MODE_SLAVE' undeclared (first use in this function); did you mean 'HAL_I2C_MODE_SLAVE'? main.c /vent_cont/Core/Src line 402 C/C++ Problem
'SPI_NSS_HARD_INPUT' undeclared (first use in this function); did you mean 'SPI_CS_MTR_Pin'? main.c /vent_cont/Core/Src line 407 C/C++ Problem
'SPI_NSS_PULSE_DISABLE' undeclared (first use in this function); did you mean 'SPI_TIMODE_DISABLE'? main.c /vent_cont/Core/Src line 413 C/C++ Problem
'SPI_NSS_PULSE_ENABLE' undeclared (first use in this function); did you mean 'I2C_NOSTRETCH_ENABLE'? main.c /vent_cont/Core/Src line 384 C/C++ Problem
'SPI_NSS_SOFT' undeclared (first use in this function); did you mean 'SPI_SR_OVR'? main.c /vent_cont/Core/Src line 377 C/C++ Problem
'SPI_PHASE_1EDGE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 376 C/C++ Problem
'SPI_PHASE_1EDGE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 406 C/C++ Problem
'TIM_MASTERSLAVEMODE_DISABLE' undeclared (first use in this function); did you mean 'TIM_AUTORELOAD_PRELOAD_DISABLE'? main.c /vent_cont/Core/Src line 507 C/C++ Problem
'TIM_MASTERSLAVEMODE_DISABLE' undeclared (first use in this function); did you mean 'TIM_AUTORELOAD_PRELOAD_DISABLE'? main.c /vent_cont/Core/Src line 544 C/C++ Problem
'TIM_OCFAST_DISABLE' undeclared (first use in this function); did you mean 'DMA_MINC_DISABLE'? motor.c /vent_cont/Core/Src line 201 C/C++ Problem
Problem
'TIM_OCPOLARITY_HIGH' undeclared (first use in this function); did you mean 'DMA_PRIORITY_HIGH'? motor.c /vent_cont/Core/Src line 200 C/C++ Problem
'TIM_TRGO_RESET' undeclared (first use in this function); did you mean 'TIM_RCR_REP'? main.c /vent_cont/Core/Src line 456 C/C++ Problem
'TIM_TRGO_RESET' undeclared (first use in this function); did you mean 'TIM_RCR_REP'? main.c /vent_cont/Core/Src line 506 C/C++ Problem
'TIM_TRGO_RESET' undeclared (first use in this function); did you mean 'TIM_RCR_REP'? main.c /vent_cont/Core/Src line 543 C/C++ Problem
'UART_ADVFEATURE_NO_INIT' undeclared (first use in this function) main.c /vent_cont/Core/Src line 569 C/C++ Problem
'UART_ADVFEATURE_NO_INIT' undeclared (first use in this function) main.c /vent_cont/Core/Src line 594 C/C++ Problem
'UART_HWCONTROL_NONE' undeclared (first use in this function); did you mean 'UART_PARITY_NONE'? main.c /vent_cont/Core/Src line 566 C/C++ Problem
'UART_HWCONTROL_NONE' undeclared (first use in this function); did you mean 'UART_PARITY_NONE'? main.c /vent_cont/Core/Src line 591 C/C++ Problem
'UART_MODE_TX_RX' undeclared (first use in this function); did you mean 'USART_TDR_TDR'? main.c /vent_cont/Core/Src line 565 C/C++ Problem
'UART_MODE_TX_RX' undeclared (first use in this function); did you mean 'USART_TDR_TDR'? main.c /vent_cont/Core/Src line 590 C/C++ Problem
'UART_ONE_BIT_SAMPLE_DISABLE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 568 C/C++ Problem
'UART_ONE_BIT_SAMPLE_DISABLE' undeclared (first use in this function) main.c /vent_cont/Core/Src line 593 C/C++ Problem
'UART_OVERSAMPLING_16' undeclared (first use in this function); did you mean 'UART_STOPBITS_1'? main.c /vent_cont/Core/Src line 567 C/C++ Problem
'UART_OVERSAMPLING_16' undeclared (first use in this function); did you mean 'UART_STOPBITS_1'? main.c /vent_cont/Core/Src line 592 C/C++ Problem
'UART_PARITY_NONE' undeclared (first use in this function); did you mean 'FLASH_PROC_NONE'? main.c /vent_cont/Core/Src line 564 C/C++ Problem
'UART_PARITY_NONE' undeclared (first use in this function); did you mean 'FLASH_PROC_NONE'? main.c /vent_cont/Core/Src line 589 C/C++ Problem
'UART_STOPBITS_1' undeclared (first use in this function) main.c /vent_cont/Core/Src line 563 C/C++ Problem
I have selected STM32FO51C8TX in the MCU selector .I have included the driver stm32f0xx_hal_spi.h,stm32f0xx_hal_tim.h,stm32f0xx_hal_uart.h file also but still i am getting the error like this. can you please tell me how to resolve this error
2020-06-20 6:47 AM
Just use the generated CubeMX code. It includes the right files. In this case, stm32f0xx.h.
2020-06-20 9:29 AM
Thanks for the reply.
I have tried this method to include the stm32f0xx_hal_spi.h file by using these steps.But still i couldn't able to resolve the error.
I am new to this controller can you please tell me how to generate the code and please tell me how o resolve the issue.
2020-06-20 10:13 AM
More of a C thing.
Make sure the Include Paths point to the right location. Do not Add .H files to the project.
Select modules in the stm32f0xx_hal_conf.h files, and add the .C library source files to the project.
2020-06-21 10:50 PM
Thanks for the reply.
I have enabled the modules in the stm32f0xx_hal_conf.h files but still i am getting error like this.
Description Resource Path Location Type
fatal error: stm32f0xx_hal_spi.h: No such file or directory stm32f0xx_hal_conf.h /Nasa_venti/Core/Inc line 273 C/C++ Problem
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:60: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.o] Error 1 Nasa_venti C/C++ Problem
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:62: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_cortex.o] Error 1 Nasa_venti C/C++ Problem
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:64: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_dma.o] Error 1 Nasa_venti C/C++ Problem
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:66: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_exti.o] Error 1 Nasa_venti C/C++ Problem
make: *** Waiting for unfinished jobs.... Nasa_venti C/C++ Problem
could you please tell me how to add the driver file stm32f0xx_hal_spi.h .
Please tell me how to resolve the issues.
2020-06-22 5:04 AM
You should only be #including stm32f0xx.h in your code, not the others. The others will get included from within that file if you have it configured correctly.
I'd recommend creating a project in STM32CubeMX, generating the code for it, and then looking at how that project is organized.
2020-06-22 6:14 AM
So if it can't find files, and you know where they are, but the compiler can't find them, it is because the INCLUDE PATHS are not being fed to the compiler properly. Check the makefile, the GNU/GCC compiler would take these as a '-I' option
Perhaps you work with someone who can guide you.
2020-07-06 5:07 AM
Thanks for the reply
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.