2019-11-15 4:01 AM
Can i transfer files from my pc to stm board memory using this config of usb memory device , else i should configure it as a host please let me know this. thanks in advance.
2019-11-15 4:32 AM
So if working fine, PC should be able to format and read/write files to MSC
2019-11-18 3:59 AM
Hi thanks for the reply , the usb memory device is only been detected as a removable disk .I am not able to format it no disk present , the size of the disk is also not available showing unknown capacity. Below is the code i have used (usb , 1Mbyte spi flash).
/////////////////////////////////usbd_storage_if.c/////////////////////////////////////////////////
#define STORAGE_LUN_NBR 1
#define STORAGE_BLK_NBR 0x100
#define STORAGE_BLK_SIZ 0x1000
int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
/* USER CODE BEGIN 6 */
for(int i =0 ;i<blk_len;i++)
{
SST80B_ReadSector(buf,0,(blk_addr*STORAGE_BLK_SIZ),STORAGE_BLK_SIZ);
buf +=STORAGE_BLK_SIZ;
}
return (USBD_OK);
/* USER CODE END 6 */
}
int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
for(int i =0; i<blk_len;i++)
{
chipsector_erase_call((blk_addr*STORAGE_BLK_SIZ));
}
for(int j =0; j<blk_len;j++)
{
SST25Write((blk_addr*STORAGE_BLK_SIZ),(uint8_t *)buf,STORAGE_BLK_SIZ);
buf +=STORAGE_BLK_SIZ;
}
}
I have configured the STORAGE_BLK_SIZ to 4096 bytes ,since the min erase of the spi flash is 4096 sector erase,
will this cause any problems.Kindly let me know .
2019-11-18 4:15 AM
You need to test your code outside of the MSC.
Both read and write routines here move data to the same block, you need to advance the block count in the loop.
Perhaps test logic on a PC C compiler where you print values. On the STM32 you could also instrument to code via a USART or SWV connection.
2019-11-20 3:59 AM
Hi thanks for the reply, i have tested the spi flash code outside msc and it is working fine , i have implemented spi flash byte read/write and sector (multi byte ) write/read as well,
uart is also added as suggested ,i am able to capture the data in the terminal while reading and writing
data into flash.
I have couple of doubts here :
STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
in the above function read and write ,i found the blk_len to be 1 , which corresponds to only one byte
why is storage read and storage write using only 1 byte transfer.
Another problem noticed here is when i configure with below :
#define STORAGE_LUN_NBR 1
#define STORAGE_BLK_NBR 0xff
#define STORAGE_BLK_SIZ 0x1000
i am not able to format , should i keep STORAGE_BLK_SIZ 0x200 .using an 1MB spi flash with
4096 byte min erase creating problems.
any inputs will be helpful,thaks in advance.
2019-11-29 3:51 AM
Hi, i was able to solve this problem, it works at 4096 block configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.