2018-08-29 11:39 PM
2018-09-01 7:29 AM
I'm assuming you're talking about the STM32F429I-DISCO, it is important you explicitly state what you have because there are a lot of boards, and it shouldn't be necessary to guess.
The DISC1 variant of the board provides a COM port with the ST-LINK.
For code running on the F429 you'd need to use the USB connector on the SOUTH end of the board (the ST-LINK being on the NORTH). The code would also need to be configured to use the USB-HS peripheral.
A review of the schematic of the board, and manual, should provide specific details of the pins.
There aren't many examples specifically for the board, this one uses Flash Drives
STM32Cube_FW_F4_V1.21.0\Projects\STM32F429I-Discovery\Applications\USB_Host\FWupgrade_Standalone
Other boards have a richer set of examples, these can be ported based on understanding of the pins/features involved.
I posted an example of using the F429-DISCO's SDRAM as a USB RAM Drive several years ago, but that used the older SPL libraries
2018-09-02 9:34 PM
hi clive, i'm using f429 discovery board. i upload the same code in 407 discovery it connected to my PC but the 429 discovery doesn't connect to PC. i don't know what's issue here. could you help me to figure it out?
2018-09-02 11:27 PM
The F407 code likely uses the USB-FS, the F429-DISCO uses the USB-HS
STM32Cube_FW_F4_V1.21.0\Projects\STM32F429I-Discovery\Applications\FatFs\FatFs_RAMDisk
STM32Cube_FW_F4_V1.21.0\Drivers\BSP\STM32F429I-Discovery\stm32f429i_discovery_sdram.c
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.