cancel
Showing results for 
Search instead for 
Did you mean: 

Hex or bin with multi-firmware

Lwang1
Associate II

My solution have more than one project, each project program in different address. exp: bootloader(0x08000000, 64K) application(0x08010000. 448K).

How can create an hex or bin with these two ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KnarfB
Super User

Most hex files can be easily combined using a text editor or simple scripts. If you're looking for tools: Python intelhex package https://python-intelhex.readthedocs.io/en/stable/

hth

KnarfB

Peter BENSCH
ST Employee

...or by using a simple text editor in which

  • you load the first hex,
  • delete the last line (usually containing :00000001FF) and then
  • append the second hex at the end

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.