cancel
Showing results for 
Search instead for 
Did you mean: 

Help with BlackPill STMF32411and Hex File for Absolute Musician Beginner for Midi Controller?

CluelessMusician
Associate

Hello!

I bought a BlackPill board, and need to upload ("flash"?) a hex-file to it.

It's for a simple musical midi controller.

I tried using Arduino once, and could copy the code to the Arduino IDE app, connect the RP Pico, and upload the code to the board, done!

I reconnect the Pico to my MacBook and the BlackPill is now a USB Midi controller.

They also have a file for the BlackPill STMF32411, in either .hex or .bin form.

I downloaded them both.

I'm on a MacBook running Big Sur.

The BlackPill has more ins and outs for switches, pots, etc., so I bought one.

Is there a simple way to upload this file to the BlackPill without allot of technical knowledge?

I should say without ANY technical knowledge?

I figured out the button sequence to put the BlackPill in bootloader mode, but the few things I tried didn't work, and frankly I don't have any idea what I am doing.

Just need to upload one of the two files to the BlackPill.

Any help would be much appreciated.

Thanks!!!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

ST resources are dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes work properly with the firmware we provide.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
CluelessMusician
Associate

I meant to mention for the Pico version of this project they provide code to paste into the Arduino IDE app. to upload to the Pico.

For the BlackPill version, they only provide either a .hex or .bin file to flash the BlackPill.

Thanks.

mƎALLEm
ST Employee

Hello,

ST resources are dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes work properly with the firmware we provide.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.