2013-08-18 10:20 PM
I want read ADC of STM32F303VC then display status on three LED (If ADC>1000 LED red bright,ADC<500 LED green bright and extant LED ogrange bright) programmed code below,but i don't find error.Thanks everyone!
#include ''main.h''__IO uint16_t AD= 0,DA=0, ADC1ConvertedVoltage = 0, calibration_value = 0;__IO uint32_t TimingDelay = 0;ADC_InitTypeDef ADC_InitStructure;ADC_CommonInitTypeDef ADC_CommonInitStructure;GPIO_InitTypeDef GPIO_InitStructure;/////////////////////////////////////////////////////////////////////////////////////////int main(void){ RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); /* Setup SysTick Timer for 1 µsec interrupts */ if (SysTick_Config(SystemCoreClock / 1000000)) { /* Capture error */ while (1) {} } ////////////////LED/////////////////////////////////// RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9| GPIO_Pin_10| GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOE, &GPIO_InitStructure); ///////////////////////ADC/////////////////////////////// /* GPIOC Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Configure ADC Channel2 as analog input (Pin 1 of Port A-PA1) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOA, &GPIO_InitStructure); ADC_StructInit(&ADC_InitStructure); //////////////////////////////////////////////////////////////////////////////////////////////// /* Calibration procedure */ ADC_VoltageRegulatorCmd(ADC1, ENABLE); /* Insert delay equal to 10 µs */ Delay(10); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1) != RESET ); calibration_value = ADC_GetCalibrationValue(ADC1); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0; ADC_CommonInit(ADC1, &ADC_CommonInitStructure); ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable; ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0; ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 1, ADC_SampleTime_4Cycles5);////////////////////////////////////////////////////////////////////////////////////////////// ADC_Cmd(ADC1, ENABLE); /* wait for ADRDY */ while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY)); ADC_StartConversion(ADC1); /* Infinite loop */ while (1) { /* Test EOC flag */ while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET); AD =ADC_GetConversionValue(ADC1); DA =(AD *3300)/0xFFF;//////////////////////////////////////////////////////////////////////////////////// while(AD>1000) { GPIO_SetBits(GPIOE,GPIO_Pin_9); } while(AD<500) { GPIO_SetBits(GPIOE,GPIO_Pin_11); } GPIO_SetBits(GPIOE,GPIO_Pin_10); }}////////////////////////////////////////////////////////////////////////////////////void Delay(__IO uint32_t nTime){ TimingDelay = nTime; while(TimingDelay != 0);}and my project here:http://www.mediafire.com/download/zbuszqh91kkah6f/ADC.7zWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.