2019-03-24 6:27 PM
I'll tell you my sad story because of a bad manipulation of the device.
Never take a call while you are sketching a project with the adc.
The LD7 turns red.
Windows detects the device and opens the usual Discovery storage unit
Maybe some technician internalized with the device has a quick idea that it could have been burned or it could guide me to check the burned component (s) in order to replace them and revive my beloved multiproposit device.
Greetings
2019-03-24 8:15 PM
Measure the voltages off the regulators.
Measure the voltages on the VCAP pins/capacitors.
Chances are you'll have to replace the F746 chip as you've likely vaporized the metalization and poly-silicon in the current's path on the die. Much better fuses than the PCB traces and gold wires.
The ST-LINK USB connection is to an F103 chip, but does suggest that 3.3V regs are working still.
2019-03-24 10:28 PM
Semiconductor Oxide thickness breakdown voltage = physics
2019-03-25 12:12 PM
This is what i measured today
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.