2023-02-22 8:47 AM
Hello,
I am Working with STM32H7 and I want to put in my board 2 QSPI as you put in your evaluation board stm32h745i-disco.
Could you say me waht is the Interface signals layout guidelines?, by the example as router clk signal (star or daisy chain).
Thank
Solved! Go to Solution.
2023-02-22 9:37 AM
Presumably the two parts will be mounted closely?
For the common CLK / NCS I'd avoid circuitous routing, just bring up a via so both top level traces are equidistance, or daisy chain one to the next as short as possible.
Try to keep the 8 data traces the same length, a 27 or 33 R series will help stop the lines ringing.
Using SOIC16W parts?
Micron has a dual die part (1Gb) allowing for both banks on one part. ST sometimes using 1x 1Gb or 2x 512Mb parts.
2023-02-22 9:37 AM
Presumably the two parts will be mounted closely?
For the common CLK / NCS I'd avoid circuitous routing, just bring up a via so both top level traces are equidistance, or daisy chain one to the next as short as possible.
Try to keep the 8 data traces the same length, a 27 or 33 R series will help stop the lines ringing.
Using SOIC16W parts?
Micron has a dual die part (1Gb) allowing for both banks on one part. ST sometimes using 1x 1Gb or 2x 512Mb parts.
2023-02-22 11:02 PM
Thank for your answer,
We are thinking to use 2x1Gb of Microm (ref. MT25QL01GBBB8E12-0SIT). This is a TBGA24. it is not SOIC.
Do you think we will have problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.