2022-03-23 4:31 AM
2022-03-23 4:34 AM
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_TSC_Init();
MX_USART1_UART_Init();
MX_USB_PCD_Init();
/* USER CODE BEGIN 2 */
BSP_EPD_Init();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
BSP_EPD_DisplayChar(0, 0, 31);
BSP_EPD_RefreshDisplay();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}The MX configuration is let by default
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.