2018-02-07 12:14 PM
Hi
I want to evaluate BlueNRG using the BlueNRG GUI. My setup is as follows:
NUCLEO-F401RE with X-NUCLEO-IDB05A1 installed. BlueNRG GUI software version V2.2.1 (latest) X-CUBE-BLE1 Cube Expansion packageI've followed the instructions found in the X-NUCLEO-IDB05A1 Quick Start Guide and copied Virtual_COM_Port_F401RE.bin the the nucleo drive.The virtual comm port appears and I can open it from BlueNRG GUI but BlueNRG GUI keeps asking:
'No Firmware detected on the motherboard. Update motherboard Firmware (under Tools menu).'
The proposed firmware installation procedure seems to be targeted at the STEVAL-IDB007V1 BlueNRG-1 development kit and fails with my setup.
Can anyone provide a hint how to get BlueNRG GUI working with the X-NUCLEO-IDB05A1?
#stm32f401re #has-no-detected #blue-nrg-gui #idb05a12018-02-16 6:38 AM
I want to connect SensorTile Board to the
BlueNRG GUI PC App but no success.
BlueNRG-MSCSP chips we purchased has old firmware and somehow none of them is working with the tile hardware we built. To test it, we want to connect the SensorTile Board via ST-LINK to the PC's
BlueNRG GUI.
Can anyone provide a hint how to get BlueNRG GUI working with the SensorTile Board?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.