2018-06-09 4:35 PM
Hi,
I'm using 2D DMA to draw sprites on the screen, but there is a surronding black color around the sprites.
So I have enabled the layer color key, and its not working, still there is a black rectangle around it.
BSP_LCD_SetColorKeying_NoReload(ActiveLayer, 0x0000);
void ConvertLineToRGB565(void * pSrc, void * pDst, uint32_t xSize, uint32_t ColorMode)
{ /* Configure the DMA2D Mode, Color Mode and output offset */ Dma2dHandler.Init.Mode = DMA2D_M2M_PFC ;//DMA2D_M2M_PFC; Dma2dHandler.Init.ColorMode = DMA2D_RGB565; Dma2dHandler.Init.OutputOffset = 0; /* Foreground Configuration */ Dma2dHandler.LayerCfg[ActiveLayer].AlphaMode = DMA2D_NO_MODIF_ALPHA; Dma2dHandler.LayerCfg[ActiveLayer].InputAlpha = 0x00; Dma2dHandler.LayerCfg[ActiveLayer].InputColorMode = ColorMode; Dma2dHandler.LayerCfg[ActiveLayer].InputOffset = 0; Dma2dHandler.Instance = DMA2D; /* DMA2D Initialization */ if(HAL_DMA2D_Init(&Dma2dHandler) == HAL_OK) { if(HAL_DMA2D_ConfigLayer(&Dma2dHandler, 1) == HAL_OK) { if (HAL_DMA2D_Start(&Dma2dHandler, (uint32_t)pSrc, (uint32_t)pDst, xSize, 1) == HAL_OK) { /* Polling For DMA transfer */ HAL_DMA2D_PollForTransfer(&Dma2dHandler, 10); } } } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.