2021-02-10 7:56 AM
Hello,
I am facing random HardFaults on a STM32F722. They happen at various places in code, sometimes even during stack's initialization.
Stack's analysis do not show any risk of overflow : most of the time, the problem happens while executing main() loop, and stack's width is never more than 2 levels.
Looking at Fault status Registers shows:
_ bit FORCED of HFSR is set to 1
_ CFSR = 0x1000000 = bit UNALIGNED of UFSR set to 1: unaligned memory access.
bit UNALIGNED_TRAP is set to 0
Looking around PC and LR, I only see "unoffensive" instructions (typically, ldr, str, or ldr.b and str.b), and the code registered in stack is part of my main's infinite loop, which most of the time executes without any trouble. So I do not understand how it could sometimes trigger a memory alignment fault...!
I read https://community.arm.com/developer/ip-products/processors/f/cortex-m-forum/43707/unable-to-determine-offending-instruction-usage-fault-illegal-unaligned-load-or-store-cortex-m7-keil-mdk-pro, and the associated links, but did not find what could trigger this fault on my board.
One track that seemed interesting was https://www.keil.com/support/docs/3777.htm, but I am not using an external SDRAM...
I also saw the following topic, which seems to be exactly the same issue than mine: https://community.st.com/s/question/0D50X00009XkiJw/stm32f7-hardfault-unaligned-memory-access?t=1612969638024. But my HCLK is at 16 MHz, so, according to STLM32F7xx's reference manual, the only latency that I can use for flash accesses is 0 WS, which is already the case...
I am using HAL for startup code and basic (while(1)) fault handlers (so I do not understand why my UsageFault escalated to HardFault, as UsageFault handler is pressent in my code).
I am using gcc and gdb with Atollic TrueStudio as IDE.
Can you please help me to solve this issue?
Regards
Solved! Go to Solution.
2021-02-11 12:51 PM
Just in case...
Note that the hard-float and soft-float ABIs are not link-compatible; you must compile your entire program with the same ABI, and link with a compatible set of libraries.
https://gcc.gnu.org/onlinedocs/gcc/ARM-Options.html
Therefore disabling FPU with -mfpu option (or adding +nofp to -march or -mcpu) also requires setting -mfloat-abi=soft.
2021-02-15 12:23 AM
Hi everyone,
Thank you for your advices.
On friday my colleague saw that some capacitors were missing on my board, and corrected this. My board has been running for the weekend, and no hardfault happened. I am leaving it running a longer time to ensure this was not luck. I also flashed another board with my software and will let it run.
I will keep you informed.
Have a nice week!
Best regards
2021-02-22 2:46 AM
Hi all,
Just to keep you in touch: I have run my software on two boards for a week, and faced no hardFault. So it seems like the problem was a hardware one.
Thank you for your advices
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.