2025-08-05 9:18 AM
Hello,
I am trying to extend DTCM to 256K. I followed FLEXMEM Configurations example but I get HardFault as soon as I try to access DTCM in 0x30020000 - 0x30040000 address range.
Could someone please provide working example of how to extend DTCM to 256K?
2025-08-05 10:05 AM
"The FLEXMEM configuration depends upon CFGDTCMSZ[3:0] and CFGITCMSZ[3:0] in SYSCFG_CM55TCMCR. It configuration cannot be changed at runtime, a reboot is needed."
https://developer.arm.com/documentation/101051/0101/Signal-descriptions/Static-configuration-signals
The POWER-ON reset might be a challenge from the debugger.
Would suggest doing without it, perhaps instrument HardFault Handler via the USART, and have success/failure indicated by LEDs, so you can observe if it faults, or that it completed the access tests.
2025-08-05 10:15 AM
Hello @IO1
This discussion should help you. See the link below.
https://community.st.com/t5/stm32-mcus-products/stm32n6-hard-fault-when-accessing-tcm/td-p/757557
Best regards,
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-06 6:38 AM - edited 2025-08-06 6:38 AM
From FLEXMEM example. How is this code supposed to work? Am I missing something here?
Writing to DTCM_ADDRESS_BASE location DTCM_SIZE_WORD times. How would that prove
that addresses other that 0x30000000 are accessible?
#define DTCM_ADDRESS_BASE 0x30000000
/* DTCM size in words : 256KB / 4 bytes per word */
#define DTCM_SIZE_WORD (256*1024 / 4 )
/* Show that memory access to DTCM is extended beyond the default 128KB */
for(int i = 0; i < DTCM_SIZE_WORD; i++)
{
uint32_t * dtcm_ptr = (uint32_t *) DTCM_ADDRESS_BASE;
*dtcm_ptr = 0xa5a5a5a5;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.