2018-10-15 12:51 AM
Dear friends,
I am trying to create a TCP server using lwIP and netconn APIs for STM32F407VGt6 MCU and recieve data from a PC software program which acts as a TCP client.
The MCU recieves all the data correctly from PC software in multiple packets and after finishing data transfer, a HardFault error occurs.
The TOTAL_HEAP_SIZE of freeRTOS is 15360 bytes and the TCP thread stack size is 256 words.
I am using CubeMX version 4.25 and HAL firmware version 1.21.0.
The code I wrote is as follows:
/* TCP_Server_Task function */
void TCP_Server_Task(void const * argument)
{
/* init code for LWIP */
MX_LWIP_Init();
/* USER CODE BEGIN 5 */
struct netconn *conn, *newconn;
err_t err, accept_err;
struct netbuf *buf;
void *data;
u16_t len;
uint8_t j;
uint8_t *tcp_rx_buf;
uint8_t length;
LWIP_UNUSED_ARG(argument);
W25Qxx_Init();
W25Qxx_SectorErase(W25QXX_BLOCK_1_ADDR);
W25Qxx_SectorErase(W25QXX_BLOCK_2_ADDR);
write_addr = W25QXX_BLOCK_2_ADDR;
/* Create a new connection identifier. */
conn = netconn_new(NETCONN_TCP);
if (conn!=NULL)
{
/* Bind connection to well known port number 502. */
err = netconn_bind(conn, IP_ADDR_ANY, 36000);
if (err == ERR_OK)
{
/* Tell connection to go into listening mode. */
netconn_listen(conn);
while (1)
{
/* Grab new connection. */
accept_err = netconn_accept(conn, &newconn);
/* Process the new connection. */
if (accept_err == ERR_OK)
{
while (netconn_recv(newconn, &buf) == ERR_OK)
{
do
{
netbuf_data(buf, &data, &len);
tcp_rx_buf = (uint8_t *)data;
length = len-1;
if(tcp_rx_buf[0] == FC_CONFIG_PROJ)
{
W25Qxx_Write(W25QXX_BLOCK_1_ADDR,&tcp_rx_buf[1],length);
}
else if(tcp_rx_buf[0] == FC_GROUP_WRITE)
{
for(j=byte_cnt ; j<len ;j++)
{
rcv_data[j] = tcp_rx_buf[j];
}
W25Qxx_Write(write_addr,&tcp_rx_buf[1],length);
W25Qxx_Read(write_addr,rcv_buff,length);
write_addr += length;
byte_cnt += length;
}
else if(tcp_rx_buf[0] == FC_PROGRAM_DONE)
{
osSignalSet(W25Qxx_ThreadHandle,1);
length = 0;
byte_cnt = 0;
write_addr = W25QXX_BLOCK_2_ADDR;
}
netconn_write(newconn, data, len, NETCONN_COPY);
}
while (netbuf_next(buf) >= 0);
netbuf_delete(buf);
}
/* Close connection and discard connection identifier. */
netconn_close(newconn);
netconn_delete(newconn);
}
}
}
else
{
netconn_delete(conn);
}
}
/* USER CODE END 5 */
}
Any helps would be appreciated.
Mutaba
2018-10-15 12:56 AM
What do the SCB registers say about the hardfault reason ?
Have you tried to narrow down the exact location, perhaps with instrumenting your code ?
2018-10-15 2:30 AM
Dear AvaTar,
thanks for your quick reply.
Yes I have checked it. HardFault is caused by MemMange and when I checked the CFSR register, the instruction access violation (IACCVIOL) flag was set.
The problem is I cannot find where exactly this happen and why.
Unfortunately the board I am using does not have a trace pin, so I cannot use trace feature.
Could you give me any ideas how to solve this problem?
2018-10-15 2:59 AM
JTAG/SWD based tracing, or an extra UART. In many cases, a single GPIO pin for toggling works.
Or you try the debugger.
> ...and after finishing data transfer, a HardFault error occurs.
I would start with the specific code parts involved.
I'm not much in Cube/RTOS code, but it sounds like a "stable" problem. Meaning consistent error at a single location.
Perhaps trying to access released/invalidated memory ?
2018-10-15 3:23 AM
Perhaps instrument malloc/free to make sure you don't have a memory leak, try to free memory twice, etc. Use a Hard Fault Handler that outputs diagnostic information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.