2014-01-17 9:09 AM
In order to test the Hard Fault interrupt, I modified the Systick example on ''STM32F0xx_Discovery_FW_V1.0.0'' as follows..
on main.c I added two lines: ------------------------------ int main(void) { uint8_t* BytePtr = (uint8_t)0x20002000; *BytePtr = 0x5a; //generate hardfault IRQ /*!< ...........comment */ /* Initialize Leds mounted on STM32F0-discovery */ STM_EVAL_LEDInit(LED3); -------------------------------------- on stm32f0xx_it.c I modified the error handler: ----------------------------------- void HardFault_Handler(void) { TimingDelay_Decrement(); //really do nothing... } --------------------------------------- So, when the line *BytePtr = 0x5a; is executed and the processor access the wrong location 0x20002000 a HardFault_Handler is called and executed. At return I expect the processor to execute the line STM_EVAL_LEDInit(LED3); but instead it returns still at line ''*BytePtr = 0x5a; and newly execute it, entering in loop!!! I am a novice on STM32 so it must be a stupid error but if I repeat the same test on the ''STM32F10x_vldiscovery_package'' it works as expected... Can someone help me?? Thanks, Luciano2014-01-17 12:50 PM
Didn't you ask this same thing last week?
That it returns to the faulting instruction doesn't seem to be overly surprising behaviour, perhaps you need to go and adjust the return PC on the stack if you want it to advance. Generally speaking the failure is considered hard, so returning is a non-optimal solution. That it behaves differently between an M0 and M3 does surprise me a little. Are you sure your M3 example is actually faulting? A read in the 0x20200000 or 0x30000000 region might be more enlightening. Perhaps you should review Joseph Yiu's books on the topic, look at the TRM, and add some diagnostic output for the assorted core registers, and stacked context?2014-01-17 12:53 PM
2014-01-17 2:28 PM
A quick skim through the TRM, User Manual, and Yiu's Essential Cortex-M0, really doesn't call this out as a difference when transitioning from an M3/4 to an M0. Arguably it should, or the state be called out more explicitly/obviously.
I haven't tested the F0, as it doesn't have SWV and I haven't wired a USART on to it, but I'm going to assume your observation is valid. I think the general expectation is that Hard Fault handlers don't return. If you don't resolve the underlying error continued execution would seem to generate some what undefined behaviour as the following code presumably expects the preceding had executed and loaded registers correctly.''Doc,'' says the patient, ''it hurts when I do this. What should I do?''
''Don't do that,'' says the physician.
2014-01-18 3:12 AM
yes but
no
satisfaction
...............2014-01-18 3:16 AM
I used this
method
to test
the amount
of RAM
present in
a chip in order to
have a portable routine
,this
works fine on
the M3
,but
it does not work
on
m0
.M3
processor loads
the PC
with address
following the
STRB
(which causes
hard
fault)
before entering the
IRQ
.M0
processor
enters
IRQ
with the PC
still
pointing
instruction
STRB
(which causes
hard
fault)
,and obviously this
causes the
loop.
Ok
, I have tochange my
routine
to avoid the problem
,but
I think this is
a
conceptual error
in the microprocessor
, do you agree
?
2014-01-18 7:00 AM
I think this is
a
conceptual error
in the microprocessor
, do you agree? More likely a design decision to reduce the complexity of the logic. Does your fault handler recognize if it's your test code that traps, or do all Hard Fault just return?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.