2018-09-12 12:31 AM
i use NUCLEO - F767ZI and test a simple code as follow
int sum(int a,int b){
return a+b;
}
int main(void){
int dly;
__enable_irq();
SysTick_Config(100000);
NVIC_EnableIRQ(SysTick_IRQn);
dly = sum(1,3);
return 0;
}i debug it and when call sum(1,3), it will goto hard fault.
if comment NVIC_EnableIRQ(SysTick_IRQn); call and it work fine.
can someone help me ?
2018-09-12 10:32 AM
The NVIC_EnableIRQ doesn't work for SysTick!!!! It doesn't have any Enable or Disable bit within NVIC. Leave all on SysTick_Config(100000); alone.
2018-09-12 11:02 AM
> The NVIC_EnableIRQ doesn't work for SysTick!!!!
Very well spotted, Tomas! - essentially the same thing Clive said but yes, it's imperative. And the comment at NVIC_EnableIRQ() says that, too.
----- [following is not reply to the original post]
Out of curiosity I had a look at NVIC_EnableIRQ() in the CMSIS headers I'm using for ages (namely
* @file core_cm4.h
* @brief CMSIS Cortex-M4 Core Peripheral Access Layer Header File
* @version V2.10
:(
static __INLINE void NVIC_EnableIRQ(IRQn_Type IRQn)
{
/* NVIC->ISER[((uint32_t)(IRQn) >> 5)] = (1 << ((uint32_t)(IRQn) & 0x1F)); enable interrupt */
NVIC->ISER[(uint32_t)((int32_t)IRQn) >> 5] = (uint32_t)(1 << ((uint32_t)((int32_t)IRQn) & (uint32_t)0x1F)); /* enable interrupt */
}Wow. IRQn_Type is an enum and signedness of that is implementation-defined; however, I don't quite get what was the benefit of the double cast (clearly it won't "heal" the improper use with SysTick and other "negative-numbered" exceptions). (In newer CMSIS the commented-out line is omitted.)
I'm apparently not alone: https://github.com/ARM-software/CMSIS_5/issues/248
JW
2018-09-12 12:27 PM
I was perhaps a little too subtle there, herding cats, should have pulled the cattle prod....
It abends because the negative pointer math is super bad.
2018-09-12 3:36 PM
In more updated CubeMX versions, it says "Value cannot be negative" in comment.
GCC compatible compiler even could assert this in compile time ( if (__builtin_constant_p(IRQn) ) _Static_assert (IRQn > 0) ... )
-- pa
2018-09-12 3:49 PM
> GCC compatible compiler even could assert
Good idea, but 1. it should be told to ARM as this is in CMSIS; 2. _Static_assert is C11, so I guess this would work only if gcc is run with some of the C11-related -std switch.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.